2019-12-05 12:54 AM
Hello, I am trying to boot kernel via TFTP from U-Boot on my DK2 board, after retrieving PXE configuration file successfully, the uImage failed to retrieved. However, I could successfully get uImage file by u-boot tftp command.
The steps I am following is https://wiki.st.com/stm32mpu/wiki/How_to_boot_the_kernel_via_TFTP_from_U-Boot#pxelinux.cfg_directory.
I have installed tftp servers on my Ubuntu, and the pxelinux.cfg directory, PXE configuration file, uImage, stm32mp157c-dk2.dtb are all under tftp directory.
/tftpboot
|---- mmc0_stm32mp157c-dk2.extlinux
| |--------- pxelinux.cfg
| |------------ 01-00-80-e1-42-51-72
| |--------- uImage
| |--------- stm32mp157c-dk2.dtb
my PXE configuration file is:
menu title Select the boot mode
DEFAULT sdcard
LABEL sdcard
KERNEL uImage
FDT stm32mp157c-dk2.dtb
APPEND root=/dev/mmcblk0p6 rootwait rw earlyprintk console=ttySTM0,115200The TF-A, u-boot, uImage, dtb file are all released by ST.
The following is the u-boot log:
STM32MP> env print ipaddr
ipaddr=192.168.1.102
STM32MP> env print ethaddr
ethaddr=00:80:e1:42:51:72
STM32MP> env print serverip
serverip=192.168.1.101
STM32MP> env print netmask
netmask=255.255.255.0
STM32MP> run bootcmd_pxe
BOOTP broadcast 1
DHCP client bound to address 192.168.1.102 (2 ms)
missing environment variable: pxeuuid
Retrieving file: /mmc0_stm32mp157c-dk2_extlinux/pxelinux.cfg/01-00-80-e1-42-51-72
Using ethernet@5800a000 device
TFTP from server 192.168.1.101; our IP address is 192.168.1.102
Filename '/mmc0_stm32mp157c-dk2_extlinux/pxelinux.cfg/01-00-80-e1-42-51-72'.
Load address: 0xc4200000
Loading: #
87.9 KiB/s
done
Bytes transferred = 181 (b5 hex)
Config file found
Select the boot mode
1: sdcard
Enter choice: 1
1: sdcard
Retrieving file: /mmc0_stm32mp157c-dk2_extlinux/uImage
Using ethernet@5800a000 device
TFTP from server 192.168.1.101; our IP address is 192.168.1.102
'.lename '/mmc0_stm32mp157c-dk2_extlinux/uImage
Load address: 0xc2000000
Loading: *
TFTP error: 'File not found' (1)
Not retrying...
for failure retrieving kernel
STM32MP> tftp mmc0_stm32mp157c-dk2_extlinux/uImage
Using ethernet@5800a000 device
TFTP from server 192.168.1.101; our IP address is 192.168.1.102
Filename 'mmc0_stm32mp157c-dk2_extlinux/uImage'.
Load address: 0xc2000000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
################################################################
1.9 MiB/s
done
Bytes transferred = 6652480 (658240 hex)
STM32MP>
Solved! Go to Solution.
2019-12-05 8:51 AM
Hi @BryanWang
Did you see this existing post :
https://community.st.com/s/question/0D50X0000BJ0vxhSQB/failed-boot-via-tftp
May it help to give solution or hints ?
Olivier
2019-12-05 8:51 AM
Hi @BryanWang
Did you see this existing post :
https://community.st.com/s/question/0D50X0000BJ0vxhSQB/failed-boot-via-tftp
May it help to give solution or hints ?
Olivier
2019-12-05 5:09 PM
Hi Olivier,
yes, this post works. Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.