2019-12-08 7:03 PM
I built the rootfs according to the instructions at https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package, but the userspace program of gcnano is not installed in the rootfs, the / vendor directory is empty.
I need to manually install gcnano-userland- multi-binary-stm32mp_6.2.4.p4-r0.0_armhf.deb to complete the installation, where is the problem
Solved! Go to Solution.
2019-12-09 6:03 PM
I think I know why,the gcnano is packaged in st-image-vendorfs-openstlinux-weston-stm32mp1.tar.xz,and i only unpackage st-image-simple-openstlinux-weston-stm32mp1-20191122051913.rootfs.tar.xz for the nfs.
so unpackage st-image-vendorfs-openstlinux-weston-stm32mp1.tar.xz into /vendor solve the issue
2019-12-09 4:47 AM
Hi @Jzhua
Did you well accept EULA when setting up the Distribution ?
Thanks
Olivier
2019-12-09 4:45 PM
yes, I accepted with the EULA
the local.conf has ACCEPT_EULA_stm32mp1 = "1"
2019-12-09 6:03 PM
I think I know why,the gcnano is packaged in st-image-vendorfs-openstlinux-weston-stm32mp1.tar.xz,and i only unpackage st-image-simple-openstlinux-weston-stm32mp1-20191122051913.rootfs.tar.xz for the nfs.
so unpackage st-image-vendorfs-openstlinux-weston-stm32mp1.tar.xz into /vendor solve the issue
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.