STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Low Power Application Question

Hello everyone!I had an application that was originally designed to run on a STM32WB55 but found it didn't have the resources we needed for it. The STM32MP1 seems like it has the potential to be a good fit for us as we could do the sensor processing ...

JayDev by Senior II
  • 3469 Views
  • 5 replies
  • 0 kudos

Resolved! USB Composite not working in STM32MP151C.

I tried to probe g_multi to make sure that USB Composite was available.modprobe g_multi file=/dev/mmcblk0The log of the probe is as follows[ 501.458553] using random self ethernet address [ 501.461560] using random host ethernet address [ 501.4806...

rmaki.1 by Associate II
  • 1756 Views
  • 1 replies
  • 1 kudos

SDIO card not found on boot

Hi,we have a custom board based on the stm32mp151c. It has on sdmmc3 a Silicon Labs WF200 Wifi Card attached. We tested this setup with the stm32mp157c-dk2 and it worked fine. Now, we do not see the message during bootup:mmc0: new high speed MMC card...

0693W000008xHn7QAE.jpg 0693W000008xHqdQAE.jpg
MScho.6 by Associate II
  • 1213 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.