cancel
Showing results for 
Search instead for 
Did you mean: 

qaudspi spi-nand flash device tree for tf-a and u-boot

ASkri.1
Senior

Hi, Everybody!

Could anyone help with correct device tree for qspi-nand flash. I can't see any activity on pins connected to flash. If I try to boot from spi-nand with BOOT0..2 set to 1, I can see clear SPI transactions... So, flash connection looks correct.

Flash type is MT29F1G01ABAFDWB

Connected to following pins:

PF10 - CLK

PB6 - NCS

PF8 - IO0

PF9 - IO1

PF7 - IO2

PF6 - IO3

TF-a device tree:

pinctrl node:
 
	qspi_bk1_pins_a: qspi-bk1-0 {
 
		pins1 {
 
			pinmux = <STM32_PINMUX('F', 8, AF10)>, /* QSPI_BK1_IO0 */
 
				 <STM32_PINMUX('F', 9, AF10)>, /* QSPI_BK1_IO1 */
 
				 <STM32_PINMUX('F', 7, AF9)>, /* QSPI_BK1_IO2 */
 
				 <STM32_PINMUX('F', 6, AF9)>; /* QSPI_BK1_IO3 */
 
			bias-disable;
 
			drive-push-pull;
 
			slew-rate = <1>;
 
		};
 
 
 
		pins2 {
 
			pinmux = <STM32_PINMUX('B', 6, AF10)>; /* QSPI_BK1_NCS */
 
			bias-pull-up;
 
			drive-push-pull;
 
			slew-rate = <1>;
 
		};
 
	};
 
 
 
	qspi_clk_pins_a: qspi-clk-0 {
 
		pins {
 
			pinmux = <STM32_PINMUX('F', 10, AF9)>; /* QSPI_CLK */
 
			bias-disable;
 
			drive-push-pull;
 
			slew-rate = <3>;
 
		};
 
	};
 
 
 
qspi node:
 
 
 
&qspi {
 
	pinctrl-names = "default";
 
	pinctrl-0 = <&qspi_clk_pins_a &qspi_bk1_pins_a>;
 
	reg = <0x58003000 0x1000>, <0x70000000 0x4000000>;
 
	#address-cells = <1>;           
 
	#size-cells = <0>;
 
	status = "okay";
 
 
 
	flash0: mt29f2g01abagd@0 {
 
		compatible = "spi-nand";
 
		reg = <0>;
 
		spi-rx-bus-width = <4>;
 
		spi-tx-bus-width = <4>;
 
		spi-max-frequency = <64000000>;
 
		#address-cells = <1>;
 
		#size-cells = <1>;
 
	};
 
};
 
 
 
u-boot device tree:
 
 
 
	qspi_clk_pins_a: qspi-clk-0 {
 
		u-boot,dm-pre-reloc;
 
		pins {
 
  		u-boot,dm-pre-reloc;
 
			pinmux = <STM32_PINMUX('F', 10, AF9)>; /* QSPI_CLK */
 
			bias-disable;
 
			drive-push-pull;
 
			slew-rate = <3>;
 
		};
 
	};
 
 
 
	qspi_clk_sleep_pins_a: qspi-clk-sleep-0 {
 
		u-boot,dm-pre-reloc;
 
		pins {
 
   		u-boot,dm-pre-reloc;
 
 			pinmux = <STM32_PINMUX('F', 10, ANALOG)>; /* QSPI_CLK */
 
		};
 
	};
 
 
 
	qspi_bk1_pins_a: qspi-bk1-0 {
 
		u-boot,dm-pre-reloc;
 
		pins1 {
 
  		u-boot,dm-pre-reloc;
 
			pinmux = <STM32_PINMUX('F', 8, AF10)>, /* QSPI_BK1_IO0 */
 
				 <STM32_PINMUX('F', 9, AF10)>, /* QSPI_BK1_IO1 */
 
				 <STM32_PINMUX('F', 7, AF9)>, /* QSPI_BK1_IO2 */
 
				 <STM32_PINMUX('F', 6, AF9)>; /* QSPI_BK1_IO3 */
 
			bias-disable;
 
			drive-push-pull;
 
			slew-rate = <1>;
 
		};
 
		pins2 {
 
    		u-boot,dm-pre-reloc;
 
			pinmux = <STM32_PINMUX('B', 6, AF10)>; /* QSPI_BK1_NCS */
 
			bias-pull-up;
 
			drive-push-pull;
 
			slew-rate = <1>;
 
		};
 
	};
 
 
 
	qspi_bk1_sleep_pins_a: qspi-bk1-sleep-0 {
 
		u-boot,dm-pre-reloc;
 
		pins {
 
   		u-boot,dm-pre-reloc;
 
			pinmux = <STM32_PINMUX('F', 8, ANALOG)>, /* QSPI_BK1_IO0 */
 
				 <STM32_PINMUX('F', 9, ANALOG)>, /* QSPI_BK1_IO1 */
 
				 <STM32_PINMUX('F', 7, ANALOG)>, /* QSPI_BK1_IO2 */
 
				 <STM32_PINMUX('F', 6, ANALOG)>, /* QSPI_BK1_IO3 */
 
				 <STM32_PINMUX('B', 6, ANALOG)>; /* QSPI_BK1_NCS */
 
		};
 
	};
 
 
 
 
 
&qspi {
 
	pinctrl-names = "default", "sleep";
 
	pinctrl-0 = <&qspi_clk_pins_a &qspi_bk1_pins_a>;
 
	pinctrl-1 = <&qspi_clk_sleep_pins_a &qspi_bk1_sleep_pins_a>;
 
	reg = <0x58003000 0x1000>, <0x70000000 0x4000000>;
 
	#address-cells = <1>;
 
	#size-cells = <0>;
 
	status = "okay";
 
 
 
	flash0: mt29f2g01abagd@0 {
 
		compatible = "spi-nand";
 
		reg = <0>;
 
		spi-rx-bus-width = <4>;
 
		spi-tx-bus-width = <4>;
 
		spi-max-frequency = <64000000>;
 
		#address-cells = <1>;
 
		#size-cells = <1>;
 
	};
 
};
 

U-boot output:

U-Boot 2020.01-stm32mp-r1 (Jan 06 2020 - 20:56:31 +0000)

CPU: STM32MP157DAB Rev.Z

Model: STMicroelectronics STM32MP157A-DK1 STM32CubeMX board

Board: stm32mp1 in trusted mode (st,stm32mp157a-stm32mp151-dk1-mx)

DRAM: 512 MiB

Clocks:

- MPU : 800 MHz

- MCU : 208.878 MHz

- AXI : 266.500 MHz

- PER : 24 MHz

- DDR : 533 MHz

WDT:  Started with servicing (32s timeout)

NAND: 0 MiB

MMC:  STM32 SD/MMC: 0

In:  serial

Out:  serial

Err:  serial

invalid MAC address in OTP 00:00:00:00:00:00

stm32 vrefbuf timed out: -110

adc@0: can't enable vdd-supply!board_check_usb_power: single shot failed for adc@0[18]!

Net:

Error: ethernet@5800a000 address not set.

No ethernet found.

Hit any key to stop autoboot: 0

Boot over usb0!

unknown raw ID d7f41b58

Error: MTD device spi-nand0 not found

DFU alt info setting: done

crq->brequest:0x0

Reset requested

#

UPLOAD ... done

Ctrl+C to exit ...

I'm completely stucked here...

Looking forward for any hints and suggestions.

Thank you in advance

Looking forward for your reply

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
PatrickF
ST Employee

Hi,

please check if you have the CLK_QSPI_ACLK in the &rcc node (TF-A Device Tree).

Regards. 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
Hi, Patrick! Thank you very much for your reply. There are more details: 1. Yes, of course we have CLK_QSPI_ACLK definition on tf-a's &rcc_node; 2. Now I can see activity on SPI pins. 3. After booting to u-boot and issuing following commands: mtdparts sf probe I've got following error message: STM32MP> sf probe unknown raw ID d7f37c30 Failed to initialize SPI flash at 0:0 (error -524) while executing sf probe commands I can see SPI-pins activity. Hardware looks ok, because spi-frequency is now set to 4Mhz and the result is the same at 2Mhz and at 48Mhz... But d7f37c30 is NOT flash ID installed - I have MT29F1G01ABAFDWB (ID: 0x2c14) - it is closest to ST examples I've found. I didn't find any NAND compatibility list, so it is not an issue. I think... After booting to linux I can see similar error message in dmesg, but now raw ID is correct: It looks like: unknown raw ID 0x002c142c Here flash ID is correct... But still unknown... But I can't provide excel log lines right now. Purpose is to get a bootable qspi-flash, but I'm still completely stuck... Thank you in advance Looking forward for you reply вт, 25 ма�? 2021 г. в 18:47, ST Community :
PatrickF
ST Employee

Hi,

maybe try putting

bias-pull-up;

for data lanes too (if not present on your PCB) instead of 'bias-disable;'

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
I will try... But't according to AN5031 external pullups is not required for data lines, except CS pin Please refer to Figure 39 Anyway I will try and send feedback to you ASAP. Thank you very much �?р, 26 ма�? 2021 г. в 19:40, ST Community :

AN5031 figure 39 show internal pull-ups, it depend on your design choice, it is either internal or external (sometimes both).

In case of boot from Serial-NAND, BootROM will setup pull-up on IO0 and IO1, but this is later override by DT settings.

I'm not sure it is the root cause (it should work without them), but easy to give it a try.

On our side, MT29F1G01ABAFD12-IT:F has been tested and it work for BootROM without fusing OTP WORD9.

Maybe worth to try with latest Ecosystem v3.0 (recommended for new design).

see also https://wiki.st.com/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board

Maybe provide TSV and complete UART console log during flashing could help too.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
Hi, Patrick! Thank you very much for your quick reply. There are following steps performed: 1. Added 10k pull-ups to all IOx, CS and CLK pins of qspi flash; 2. Modified DT. I have added current DT nodes to the end of this letter; 3. All tested again. Here is TSV file generated for SPI nand: #Opt Id Name Type IP Offset Binary - 0x01 fsbl1-boot Binary none 0x0 ../../arm-trusted-firmware/tf-a-stm32mp157a-stm32mp151-dk1-mx-serialboot.stm32 - 0x03 ssbl-boot Binary none 0x0 ../../bootloader/u-boot-stm32mp157a-stm32mp151-dk1-mx-trusted.stm32 P 0x04 fsbl1 Binary(2) nand0 0x00000000 ../../arm-trusted-firmware/tf-a-stm32mp157a-stm32mp151-dk1-mx-trusted.stm32 P 0x06 ssbl Binary nand0 0x00200000 ../../bootloader/u-boot-stm32mp157a-stm32mp151-dk1-mx-trusted.stm32 P 0x07 ssbl2 Binary nand0 0x00400000 ../../bootloader/u-boot-stm32mp157a-stm32mp151-dk1-mx-trusted.stm32 P 0x21 ubifs System nand0 0x00600000 ../../st-image-weston-openstlinux-weston-stm32mp1-disco-mx_nand_4_256_multivolume.ubi Here is console output I'm trying to load it to board: U-Boot 2020.01-stm32mp-r1 (Jan 06 2020 - 20:56:31 +0000) CPU: STM32MP157DAB Rev.Z Model: STMicroelectronics STM32MP157A-DK1 STM32CubeMX board Board: stm32mp1 in trusted mode (st,stm32mp157a-stm32mp151-dk1-mx) DRAM: 512 MiB Clocks: - MPU : 800 MHz - MCU : 208.878 MHz - AXI : 266.500 MHz - PER : 24 MHz - DDR : 533 MHz WDT: Started with servicing (32s timeout) *NAND: 0 MiB*MMC: STM32 SD/MMC: 0 In: serial Out: serial Err: serial invalid MAC address in OTP 00:00:00:00:00:00 stm32 vrefbuf timed out: -110 adc@0: can't enable vdd-supply!board_check_usb_power: single shot failed for adc@0[18]! Net: Error: ethernet@5800a000 address not set. No ethernet found. Hit any key to stop autoboot: 0 Boot over usb0! *unknown raw ID d7f41ba8Error: MTD device nand0 not found*DFU alt info setting: done crq->brequest:0x0 Reset requested # UPLOAD ... done Ctrl+C to exit ... If I continue to load linux kernel from eMMC connected, I'm getting following dmesg messages related to nand: root@stm32mp1-disco-mx:~# dmesg | grep spi [ 2.658599] spi-nand spi0.0: unknown raw ID ff*2c14*2c [ 2.662127] spi-nand: probe of spi0.0 failed with error -524 2�?14 here is the correct flash_id. But I don't know ff before and 2c again after... Also have no Ideas why :) SPI speed is 4Mhz only to avoid possible hardware problems. Here is DT nodes related to qspi: TF-A: quadspi_pins_mx: quadspi_mx-0 { pins1 { pinmux = , /* QUADSPI_BK1_NCS */ , /* QUADSPI_BK1_IO3 */ , /* QUADSPI_BK1_IO2 */ , /* QUADSPI_BK1_IO0 */ ; /* QUADSPI_BK1_IO1 */ // bias-disable; bias-pull-up; drive-push-pull; slew-rate = <1>; }; pins2 { pinmux = ; /* QUADSPI_CLK */ bias-pull-up; // bias-disable; drive-push-pull; slew-rate = <2>; }; }; &qspi { pinctrl-names = "default"; pinctrl-0 = <&quadspi_pins_mx>; reg = <0x58003000 0x1000>, <0x70000000 0x8000000>; #address-cells = <1>; #size-cells = <0>; status = "okay"; nand0: mt29f1g01abafd@0 { compatible = "spi-nand"; reg = <0>; spi-rx-bus-width = <4>; spi-tx-bus-width = <4>; spi-max-frequency = <4000000>; #address-cells = <1>; #size-cells = <1>; }; }; u-boot & linux: quadspi_pins_mx: quadspi_mx-0 { u-boot,dm-pre-reloc; pins1 { u-boot,dm-pre-reloc; pinmux = , /* QUADSPI_BK1_NCS */ , /* QUADSPI_BK1_IO3 */ , /* QUADSPI_BK1_IO2 */ , /* QUADSPI_BK1_IO0 */ ; /* QUADSPI_BK1_IO1 */ // bias-disable; bias-pull-up; drive-push-pull; slew-rate = <1>; }; pins2 { u-boot,dm-pre-reloc; pinmux = ; /* QUADSPI_CLK */ // bias-disable; bias-pull-up; drive-push-pull; slew-rate = <2>; }; }; quadspi_sleep_pins_mx: quadspi_sleep_mx-0 { u-boot,dm-pre-reloc; pins { u-boot,dm-pre-reloc; pinmux = , /* QUADSPI_BK1_NCS */ , /* QUADSPI_BK1_IO3 */ , /* QUADSPI_BK1_IO2 */ , /* QUADSPI_BK1_IO0 */ , /* QUADSPI_BK1_IO1 */ ; /* QUADSPI_CLK */ }; }; &qspi { u-boot,dm-pre-reloc; pinctrl-names = "default", "sleep"; pinctrl-0 = <&quadspi_pins_mx>; pinctrl-1 = <&quadspi_sleep_pins_mx>; reg = <0x58003000 0x1000>, <0x70000000 0x8000000>; #address-cells = <1>; #size-cells = <0>; status = "okay"; nand0: mt29f1g01abafd@0 { u-boot,dm-pre-reloc; compatible = "spi-nand"; reg = <0>; spi-rx-bus-width = <4>; spi-tx-bus-width = <4>; spi-max-frequency = <4000000>; #address-cells = <1>; #size-cells = <1>; }; }; qspi clock is enabled in &rcc_node for both TF-A and U-BOOT: st,pkcs = < CLK_CKPER_HSE // CLK_ETH_PLL4P * CLK_QSPI_ACLK* CLK_ETH_DISABLED CLK_SDMMC12_PLL4P Distribution package is: openstlinux-5.4-dunfell-mp1-20-06-24 Should I compile u-boot myself? :) Thank you in advance Looking forward for your repl чт, 27 ма�? 2021 г. в 09:31, ST Community :
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.