STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RPMSG SDB cached buffer

We follow this: https://wiki.st.com/stm32mpu/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_principle and this: https://wiki.st.com/stm32mpu/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_example#Linux_driversarticles...

mishuk by Associate III
  • 2965 Views
  • 4 replies
  • 0 kudos

Resolved! STM32MP1waking from Standby by WAKE UP pins

Hello everyone!I’ve tested wake up from standby mode with Wake up pins PI11 (and PI8). But it is not work I have remove all definitions about wake up pins in dts except place where it defines as wake up pins in stm32mp151.dtsi Entering in standby mod...

AKudr.1 by Associate II
  • 2383 Views
  • 2 replies
  • 0 kudos

Resolved! Cannot use GPU on a custom board.

We boot up the odyssey Stm32mp157c board with distribution package. While booting the display is working but when i try to run qt examples it gives core dump error. Also there is no connector or encoder in the output of modetest. I could't figure out...

EKIRT.1 by Associate II
  • 10601 Views
  • 7 replies
  • 0 kudos

Resolved! barebox I2C4 access

Hello,we try to access the I2C4-Bus under barebox, we use:CPU: STM32MP151CAA Rev.ZTF-A: v2.4-r1.0-nofip(release):b5d0088b9-dirtybarebox: barebox 2021.04.0-02204-gaa9b7b34b8e-dirtyIn the TF-A the I2C4 is unlocked by: DECPROT(STM32MP1_ETZPC_I2C4_ID, DE...

RGlie.1 by Associate II
  • 3026 Views
  • 4 replies
  • 0 kudos

Can not controll GPIO from Kernel Space

Hello i wanted to use the GPIOLib to control my pin manualy. so i added this in my device tree.&usart3 { pinctrl-names = "default", "sleep", "idle"; pinctrl-0 = <&usart3_pins_c>; pinctrl-1 = <&usart3_sleep_pins_c>; pinctrl-2 = <&usart3_idle_pins_c>; ...

SAman.1 by Associate III
  • 3716 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.