STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32mp1 pin mux in kernel dts

currently i have a pin <STM32_PINMUX('F', 14, GPIO)> how to mux as a GPIO before using as a gpiolib, export work fine, but i2c4 is not working but i can see GPIO is getting based on sys gpiolib. as before export i see PF14 line is muxed as pin 94 (P...

Ara.1 by Senior
  • 1947 Views
  • 5 replies
  • 0 kudos

How do i run a custom built DDR_Test_Suite (U-Boot.SPL.STM32MP157C-DK2.stm32) using CubeMX?

I am trying to verify my build environment by building the U-boot code samples to be able to run the DDR Tuning tests.First I start CubeMX (using the ubuntu image provided on one of your workshops) and under tools i choose the DDR Test Suite and sele...

DOlss.1 by Associate II
  • 4999 Views
  • 6 replies
  • 3 kudos

Resolved! It's possible to make work USB-OTG and USART1 in the same device (STM32MP157CAC)?

Hi everyone.I have an already-designed PCB with an STM32MP157 on it. In order to communicate with an external device, I am using USART1. At the same time, I'm using an USB OTG port to connect my device to my PC.My problem is that USART1 is working wi...

areify by Associate II
  • 13803 Views
  • 12 replies
  • 0 kudos

Parallel programming STM32MP157F

Hello everyone,I've a question. If I'm not confused, STM32MP157F is dual CA7 core. Now, I'm coding a Linux application which I would like to parallelize. How can I do it? Is there any kind of directives such as OpenMP?Thanks,Oscar

OBaselga by Associate III
  • 1042 Views
  • 0 replies
  • 0 kudos

Resolved! GPIO Interrupts on STM32MP1

Hi,I am trying to interface a rotary encoder to A7 on STM32MP1.I was able to get the CubeMx COnfiguration done and got the device tree file generated.Also looked into this document: https://wiki.st.com/stm32mpu/wiki/Interrupt_overview#pinctrl_irqchip...

NPal.2 by Senior
  • 3126 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.