2021-09-07 4:07 AM
Hey guys,
Having some issues with running through the kernel setup and dont understand the errors returned back as iv followed all the steps to a T.
Attached my terminal history. This in on the https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7/Modify,_rebuild_and_reload_the_Linux%C2%AE_kernel
I honestly dont understand what i may have done wrong here. if possible id like to understand the method to understanding errors within linux as this is my first ish run with native linux installed
Also to note i did have a look at the readmes within the file system to which i think they differ slightly to whats whats on the wiki.
Error:
andreas@andreas-desktop:~/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Developer-Package/en.SOURCES-kernel-stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10$ make -j2 ARCH=arm modules
CC scripts/mod/empty.o
HOSTCC scripts/mod/mk_elfconfig
gcc: error: unrecognized argument in option ‘-mabi=aapcs-linux’
gcc: note: valid arguments to ‘-mabi=’ are: ms sysv
gcc: error: unrecognized command line option ‘-mlittle-endian’
gcc: error: unrecognized command line option ‘-mfpu=vfp’
make[1]: *** [scripts/Makefile.build:279: scripts/mod/empty.o] Error 1
make[1]: *** Waiting for unfinished jobs....
make: *** [Makefile:1205: prepare0] Error 2
andreas@andreas-desktop:~/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Developer-Package/en.SOURCES-kernel-stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10$ mkdir -p $PWD/install_artifact/
andreas@andreas-desktop:~/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Developer-Package/en.SOURCES-kernel-stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10$ make ARCH=arm INSTALL_MOD_PATH="$PWD/install_artifact" modules_install
sed: can't read modules.order: No such file or directory
make: *** [Makefile:1425: _modinst_] Error 2
andreas@andreas-desktop:~/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Developer-Package/en.SOURCES-kernel-stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10$ make -j2 ARCH=arm uImage vmlinux dtbs LOADADDR=0xC2000040
CC scripts/mod/empty.o
CC scripts/mod/devicetable-offsets.s
gcc: error: unrecognized argument in option ‘-mabi=aapcs-linux’
gcc: note: valid arguments to ‘-mabi=’ are: ms sysv
gcc: error: unrecognized argument in option ‘-mabi=aapcs-linux’
gcc: note: valid arguments to ‘-mabi=’ are: ms sysv
gcc: error: unrecognized command line option ‘-mlittle-endian’
gcc: error: unrecognized command line option ‘-mlittle-endian’
gcc: error: unrecognized command line option ‘-mfpu=vfp’
make[1]: *** [scripts/Makefile.build:279: scripts/mod/empty.o] Error 1
make[1]: *** Waiting for unfinished jobs....
gcc: error: unrecognized command line option ‘-mfpu=vfp’
make[1]: *** [scripts/Makefile.build:117: scripts/mod/devicetable-offsets.s] Error 1
make: *** [Makefile:1205: prepare0] Error 2
Solved! Go to Solution.
2021-09-07 4:18 AM
Hello @AMeta
It seems to me your environment is not correctly set and you are using the native gcc compiler.
Did you setup the SDK environment as explained in this wiki page? https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7/Install_the_SDK
Best regards
--JM
2021-09-07 4:18 AM
Hello @AMeta
It seems to me your environment is not correctly set and you are using the native gcc compiler.
Did you setup the SDK environment as explained in this wiki page? https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7/Install_the_SDK
Best regards
--JM
2021-09-07 6:18 PM
Thanks jean, there was an error on one of the commands i must of made on setup that i missed.
appreciate it !!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.