cancel
Showing results for 
Search instead for 
Did you mean: 

How to connect the stm32mpu157f-dk2 and the amicam1?

JJérô.1
Associate II

@Alain FERRARI​ 

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Olivier GALLIEN
ST Employee

Hi @JACQUES Jérôme​ ,

Sorry this kind of post is not really constructive.

Thanks to avoid to mention directly ST people except if it's to answer to one of their comment.

Thanks to elaborate in the body all information that help to get context and allow community to understand the request.

If I correct the typo I understand you talk about X-NUCLEO-AMICAM1 ? Right ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Hello,
Yes, in fact il would like to connect the amicam1 with the stm32mp157f-dk2.
I have configured the amicam1 to accept 4 mems microphones(mic0007v1).
On the other way, i would like to connect a arducam fort example the imx477.
Is it possible?
Best regards
Olivier GALLIEN
ST Employee

Hi @JACQUES Jérôme​ ,

Don't know but I think this article might give you all the steps to evaluate and proceed if possible :

https://wiki.st.com/stm32mpu/wiki/IKS01Ax_MEMS_expansion_board

Hope it help

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Hi Olivier,
Thanks.
I have read this article and try to do the same.
But the difficulty is to modify the kernel tree and to have the possibility to control with a gui the amicam.
Best regards
Le 19/07/2022 à 16:23, ST Community a écrit :
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.