STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Attempting to build from my custom device trees generated by CubeMX and getting this error "fatal error: stm32mp15-m4-srm.dtsi: No such file or directory" at the OP-TEE build stage.

I've written a script that basically builds everything based on this wiki - wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package#Updating_the_kernel_device_treeWith the script I can successfully build from the existing ...

JKell.6 by Associate III
  • 1501 Views
  • 4 replies
  • 0 kudos

Resolved! STM32MP157A-DK1 StLink LED is always red

Hi,When I power on my STM32MP157A-DK1 board, ST-LINK LED (LD4) is always red. On my Linux system when I connect the board through ST-LINK micro usb port (CN11), it is only detected as 'STM32 Virtual ComPort', and not detected as StLink device. And wh...

fyildirim by Associate II
  • 8398 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.