2022-12-08 9:28 AM
Is there any STM MCU/MPU which can be used for computer vision applications such as face recognition, Object detection/tracking? If so, how much flash memory required to process video with 5MP camera at 30FPS?
Is there any STM MCU/MPU which can be used for AR/VR applications?
2022-12-09 10:23 AM
The STM32MP series is more suited. But even more suited would be a full blown computer.
5MP * 30fps * 3bpp = 3.6 GBps. Not processing that on an MCU.
2023-01-06 7:12 AM
Hi @NPete.3
please have a look to https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_OpenSTLinux_Expansion_Package
and more specifically https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_-_face_recognition_using_TensorFlow_Lite_C%2B%2B_API
Regards,
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.