STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! extlinux.conf can't chose uInitrd boot

hi st expert​I am porting openstlinux for my robot board, I found that the system froze after uboot selected the extlinux file, and then rebooted after a while,the uart log :Do I have any debugging means to analyze where the current problem is? than...

0693W00000aIpSSQA0.png 0693W00000aIpnJQAS.png
ttao.1 by Associate II
  • 2385 Views
  • 2 replies
  • 0 kudos

Resolved! How to get terminal on STM32MP157D-EV1? The COM port cann't be seen from the host PC.

The board is set up as follows, and USB of ST-Link V2-1 is connected to Host PC.   when using Linux host pc , /dev/ATM* devices not recognized.So I used a Windows PC, but it is not recognized either.Do I need to install a special driver to recognize ...

0693W00000D0cO8QAJ.jpg 0693W00000D0cJOQAZ.jpg
HKim.23 by Associate III
  • 3677 Views
  • 9 replies
  • 0 kudos

Resolved! Getting error/warning "Gtk-WARNING **: 18:09:46.325: cannot open display:" while executing "hello-world" sample application with STM32MP157F-DK2. Expected a GTK window is NOT displayed on display screen

Hi, I'm getting error "(gtk_hello_world:1474): Gtk-WARNING **: 18:09:46.325: cannot open display: " while executing "hello-world" sample application with STM32MP157F-DK2. Expected a GTK window is NOT displayed on display screenI have followed steps a...

S.Kamath by Associate III
  • 5526 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.