STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MIPI display blank after enabling uart8

I'm using a custom stm32mp157a board with a DSI display.If I enable uart8 using pins J8 (UART8_TX) and J9 (UART8_RX) the display driver (panel-sitronix-st7701.c) doesnt load properly and the display stays blank. uart8 does work properly. If I disab...

Rc.1 by Associate II
  • 1853 Views
  • 1 replies
  • 0 kudos

Resolved! OPTEE Core data-abort problem.

We recently udated from OpenSTLinux v2.1 to v4.1. The boot chain is solid, but occasionally we are getting TEE aborts (trace listed below). I am not sure exactly how to debug this, any help would be appreciated. E/TC:1 E/TC:1  Core data-abort a...

Macdog by Associate III
  • 4401 Views
  • 3 replies
  • 0 kudos

Custom board openstlinux distribution problem

Hi there, I am building custom board with openstlinux distribution package with following configBuild Configuration:BB_VERSION          = "2.0.0"BUILD_SYS           = "x86_64-linux"NATIVELSBSTRING     = "universal"TARGET_SYS          = "arm-ostl-linu...

Resolved! SDK installation script

Hello,I would like to setup environment for STM32MPU according this instruction:https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7/Install_the_SDKso I downloaded the SDK .tar https:/...

ZHala.1 by Associate II
  • 10131 Views
  • 9 replies
  • 0 kudos

Resolved! SciPy and Librosa libraries on ST MP1 Linux

Hello,I’m using an ST MP1 Development Kit STM32MP157C-DK2 to develop and deploy projects involving Machine Learning on an SoC.I need to perform some pre-processing operations on data coming from different sensors and to do so I have at my disposal Py...

pignaz by Associate
  • 3196 Views
  • 1 replies
  • 0 kudos

Can I use sd card programmed on stm32mp157f-dk2 board on custum board(embedded stm32mp157d)?

I have two boards stm32mp157f-dk2 and my custum board(embedded stm32mp157d).I know that the difference stm32mp157f and stm32mp157d is simply security part.And my custom board don't have C-type connector because of issues in parts supply.So, After plu...

SKim.36 by Associate II
  • 2253 Views
  • 1 replies
  • 0 kudos

The STM32MP157 is configured for ADC acquisition within the M4 core, and the ADC data is carried using the DMA method. It turns out that the sample rate and the sampled data are correct when debugging with the development board MCU start-up method Debug,

The two graphs above are the data obtained from different cores. The left side is the MCU method start, the sampling rate is 1.6M, the acquisition of 1KHz signal, the acquisition of 1600 points is correct; the right side is the EMMC from the A7 core ...

kh_placeholder.png
ybai.2 by Associate
  • 2637 Views
  • 2 replies
  • 0 kudos

Resolved! Is there an example of how to perform DDR data bit swapping as described in AN5122?

We are using LPDDR2 and have wired the data bits as per the ST provided example STM32MP15XXAD_LPDDR2x16-Example-A01_Schematic.PDF (attached)We have swapped the same bits in the DQ15:8 byte as per the PDF but I can't find anything to tell me how to pe...

_legacyfs_online_stmicro_images_0693W00000bifUDQAY.png
damien1 by Associate II
  • 2950 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.