STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP133D optee issue.

Hello.I am on porting STM32MP135F-DK Discovery Board source to STM32MP133D based customizing board.With bitbake build, the firmwares work well with STM32MP135F-DK.But with our developing board, it stuck on BL2 boot with panic. The main difference is ...

capture.JPG
ritoseo by Associate
  • 3179 Views
  • 2 replies
  • 0 kudos

Resolved! Text editor

Hi,Does exist inside the Discovery kit with STM32MP135F board a text editor like nano or wim ?And if not how can I install it ?Thank you.Olivier.

Olivier73 by Associate II
  • 3957 Views
  • 5 replies
  • 1 kudos

Resolved! Networks settings

Hi, Each time I reboot my Discovery kit with STM32MP135F borad I lost the network (IP V4 address). How can I set the IP address, Does exits somewhere a /etc/network/interface file ? Thank you, Olivier.    

Olivier73 by Associate II
  • 2672 Views
  • 3 replies
  • 0 kudos

Resolved! OTP Bits Cannnot read

Hi All.I use discovery board of STM32MP157F-DK2 .So I want t to try  read OTP Bits via STM32CubeProgrammer , But I find 2 errs.The err things search ST Community, I fund it. Can't read OTP bits on STM32MP157C-DK2 using STM32CubeProgrammer So I Try to...

Yocto ST-linux headless distribution

Hi there, I'm building an ST-Linux distribution with Yocto (ST Distribution package) on a custom board (based on STM32MP153), and, now that I've tested it, I need to optimize the final image.My distribution should be completely headless (so no HMI an...

SScar.2 by Senior
  • 1433 Views
  • 0 replies
  • 0 kudos

Resolved! run Weston fail on Buildroot

 Hi,The MP157F-DK2 comes with an SD card attached. Weston (ver 5.0.0) with DRM works well.But if I want to run Weston(ver 10.0.1) on Buildroot, it will fail.Do I need to build more packages for Weston?I am using the version of Buildroot.a. buildroot:...

wG.1 by Associate II
  • 3813 Views
  • 1 replies
  • 1 kudos

Seeking Guidance on Using Altium Designer for STM32 PCB using it's design files directly

  *I've imported successfully of STM32mp157 dk-1 board 's schematics in altium designer and I don't know whether this processor is over advanced for application or it is must need to use for our product. even though I'm newbie with lesser yr of exp ,...

mbed_engr by Associate II
  • 5333 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.