2024-05-07 5:45 AM
Hi Team,
I am facing issue 5.15.67 kernel version.
Starting kernel ...
E/TC:0 Panic 'Watchdog' at core/drivers/stm32_iwdg.c:105 <stm32_iwdg_it_handler>
E/TC:0 TEE load address @ 0xfe200000
E/TC:0 Call stack:
E/TC:0 0xfe203cb5
E/TC:0 0xfe21b32d
E/TC:0 0xfe20ec3d
E/TC:0 0xfe21a9ed
E/TC:0 0xfe237f07
E/TC:0 0xfe200340
Can anybody know this fix solution please pro
Regards,
Sateesh
2024-05-07 5:26 PM
Hello @SATEESH_52
This post has been escalated to the ST Online Support Team for additional assistance.
We'll contact you directly.
Regards,
Roger
2024-05-14 11:29 PM - edited 2024-05-14 11:29 PM
Hello Team,
I posted this issue 10days back still I not get any reply. Can anybody take initiative and respond my issue.
2024-05-15 4:48 AM
Hi @SATEESH_52
Could you please provide more information on your setup ?
Why did you conclude issue is from WIFI driver when there seems to be a watchdog interrupt going to OpTee ?
Which STM32MP1 device ? Which board ?
Which ecosystem version (seems v4.1.00 according to kernel version) and if individual components (TF-A, uBoot, Optee) are the right one for this ecosystem version ?
Full console log ?
Regards.
2024-05-19 10:23 PM
Hi PatrickF,
I am not concluding wifi driver issue. This releated to OPTEE. Which I was using custom board (STM32MP133C)
optee version - a1f02f4f3daae7e21ee58b4c93ec3e46b8f28d15 (HEAD -> master, tag: v2.6-rc1, tag: v2.6)
kernel version - 1.15.67
2024-05-20 2:26 AM
Hello @SATEESH_52 ,
It looks that your kernel just does not start, and so is not able to kick the OPTEE watchdog, that leads to a watchdog panic in OPTEE. (Linux is responsible to regularly kick an OPTEE watchdog that is a kind of heartbeat to check if the link is still alive).
So you have to find why does your Linux kernel not start.
Can you double check that all your SW component are aligned with the version waited with OpenSTLinux v4.1 ? (you can check the versions at this link : https://wiki.st.com/stm32mpu-ecosystem-v4/wiki/STM32_MPU_OpenSTLinux_release_note_-_v4.1.0#Release_content).
Kind regards,
Erwan.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.