2024-10-01 6:04 AM
Hi there TouchGFX team
I've a ui running on the simulator and I would like to start running it on my dk. I can't find any examples on how to run it on the stm32mp135-dk, can you me guide on this?
Thanks a lot in advance
Solved! Go to Solution.
2024-10-03 2:39 AM
Hello @JPabl.1,
The X-TOUCHGFX-MPU Add-on is based on STM32Cube BareMetal Ecosystem.
There a getting started section in ST Wiki page which would help you to start your first TouchGFX project on STM32MP135F-DK board.
How to install X-TouchGFX MPU Addon - stm32mpu
You might also need to look on official TouchGFX Documentation to get better knowledge about how to develop GUI with TouchGFX framework.
Introduction | TouchGFX Documentation
You can use any of the available examples on the TouchGFX Designer Tool which is compatible with the STM32MP135F-DK board. Please refer to section "5.1. TouchGFX Quick Start" in the ST Wiki page mentioned above for more details.
Unfortunately, as far as I know you can't deploy your pre-built TouchGFX application (BareMetal based app) on your Linux based platform, this won't work on your target. This wouldn't work as the application will be running on the same main processor CA7.
If you have logs about the error, you have got while trying to build your TouchGFX app with STM32CubeIDE please post it here we can try to help you fixing them.
Best Regards,
Akram
2024-10-02 9:32 AM
Hello,
This wiki can help you.
2024-10-02 11:06 AM
Thanks for the quick reply.
I followed that wiki and although I haven't been able to compile the project in STM32Cube IDE it helped solve some questions.
This "add on" works as a bare metal application? I'm using the MPU so I intend to run embedded Linux on it, and the idea is to develop the GUI using TouchGFX.
It seems this "add on" is very new, so I haven't found any documentation or examples about it. I'm still confused if I can develop my GUI on TouchGFX, add my business logic using STM32Cube IDE, compile it and add it to my embedded Linux image. is this approach possible?
Thanks!
2024-10-03 2:39 AM
Hello @JPabl.1,
The X-TOUCHGFX-MPU Add-on is based on STM32Cube BareMetal Ecosystem.
There a getting started section in ST Wiki page which would help you to start your first TouchGFX project on STM32MP135F-DK board.
How to install X-TouchGFX MPU Addon - stm32mpu
You might also need to look on official TouchGFX Documentation to get better knowledge about how to develop GUI with TouchGFX framework.
Introduction | TouchGFX Documentation
You can use any of the available examples on the TouchGFX Designer Tool which is compatible with the STM32MP135F-DK board. Please refer to section "5.1. TouchGFX Quick Start" in the ST Wiki page mentioned above for more details.
Unfortunately, as far as I know you can't deploy your pre-built TouchGFX application (BareMetal based app) on your Linux based platform, this won't work on your target. This wouldn't work as the application will be running on the same main processor CA7.
If you have logs about the error, you have got while trying to build your TouchGFX app with STM32CubeIDE please post it here we can try to help you fixing them.
Best Regards,
Akram
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.