2021-06-02 8:50 AM
We use the STM32MP157CA and the STM32CubeIDE and let the code generator generate a confiuration with the required modules. In our case the SPI1 on the pins (PZ0,PZ1,PZ2). The generated functions provide the initializations for the SPI1. Unfortunately the SPI1 does not work for us in normal operation mode. If we call the HAL_SPI_Transmit(...) function after the initialization we get a SPI timeout. On the oscilloscope we see no clock on the spi clock line. We also noticed that when we use the engineering mode for the M4 the SPI1 works.
If we change the SPI to the SPI5 (also generated with the code generator) everything works in normal operation mode and in engineering mode. How can we use the SPI1 in normal operation mode on the M4?
Solved! Go to Solution.
2021-06-09 7:16 AM
Hi,
could you check that in your uBoot and kernel DT, you have this line?
#include "stm32mp15-m4-srm.dtsi"This will include other file which contain important DT declaration for M4 assigned peripherals.
like this one https://github.com/STMicroelectronics/linux/blob/v5.10-stm32mp/arch/arm/boot/dts/stm32mp15-m4-srm.dtsi
Regards.
2021-06-10 3:02 AM
Hello PatrickF,
i have check the uBoot and kernel DT. Both have the
#include "stm32mp15-m4-srm.dtsiline.
But my console Message do not include the
[xxxx.xxxx] rproc-srm-core 10000000.m4:m4_system_resources: bound 10000000.m4:m4_system_resources:spi@44004000 (ops xxxx)lines when i start the M4.
Mine look like this:
remoteproc remoteproc0: Booting fw image MP1M4-SP00261.elf, size 3542808
[ 145.357067] mlahb:m4@10000000#vdev0buffer: assigned reserved memory node vdev0buffer@10042000
[ 145.367638] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 145.372194] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty-channel addr 0x0
[ 145.380111] mlahb:m4@10000000#vdev0buffer: registered virtio0 (type 7)
[ 145.386751] rpmsg_tty virtio0.rpmsg-tty-channel.-1.0: new channel: 0x400 -> 0x0 : ttyRPMSG0
[ 145.387483] remoteproc remoteproc0: remote processor m4 is now up
[ 145.409260] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty-channel addr 0x1
[ 145.419239] rpmsg_tty virtio0.rpmsg-tty-channel.-1.1: new channel: 0x401 -> 0x1 : ttyRPMSG1
[ 145.435174] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty-channel addr 0x2
[ 145.453165] rpmsg_tty virtio0.rpmsg-tty-channel.-1.2: new channel: 0x402 -> 0x2 : ttyRPMSG2Only our 3 RPMSG channels are displayed as a message.
2021-06-10 5:12 AM
So, after M4 FW is started, when you enter:
cat /proc/device-tree/ahb/m4@10000000/m4_system_resources/spi@44004000/statusyou probably get 'disabled'.
It is likely that the parsed kernel device tree miss the &m4_spi1 node.
Please double check if you compile and use the right device trees.
in uBoot log, you should have something like
Retrieving file: /stm32mp157c-xxxx.dtbIf not the expected file, please check extlinux.conf, not clear to me how it works for custom board, but for sure it could end up that Linux not using the right DT.
Regards.
2021-06-10 5:45 AM
Hello PatrickF,
i check the spi1 status when the M4 is running wih:
cat /proc/device-tree/mlahb/m4@10000000/m4_system_resources/spi@44004000/statusand get "okay".
Yes our custom dtb gets loaded at boot.
To check the device tree i copy the kernel device tree from /boot and "decompile" the dtb with:
dtc -I dtb -O dts -o decompiled.dts stm32mp157c-hp00164.dtbThe dts contains entries for spi@4400400:
/ {
...
soc {
...
spi@44004000 {
#address-cells = <0x01>;
#size-cells = <0x00>;
compatible = "st,stm32h7-spi";
reg = <0x44004000 0x400>;
interrupts = <0x00 0x23 0x04>;
clocks = <0x01 0x82>;
resets = <0x01 0x4c48>;
dmas = <0x0c 0x25 0x400 0x01 0x0c 0x26 0x400 0x01>;
dma-names = "rx\0tx";
power-domains = <0x0d>;
status = "disabled";
};
...
}
...
mlahb {
...
m4@10000000 {
...
m4_system_resources {
...
spi@44004000 {
compatible = "rproc-srm-dev";
reg = <0x44004000 0x400>;
clocks = <0x01 0x82>;
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <0x5e>;
};
...
}
...
}
}
2021-06-10 7:36 AM
Hi,
could you also check if
cat /proc/device-tree/ahb/m4@10000000/m4_system_resources/statusreturn 'okay' too ?
In case you rebuilt the kernel, please check if the following config are enabled (they are ON by default in the starter package):
Regards.
2021-06-10 8:55 AM
Hello PatrickF,
i check the m4_system_resurces status with:
cat /proc/device-tree/mlahb/m4@10000000/m4_system_resources/statusbut it returns "disabled" when the M4 is running.
I also check the config for my actual running kernel with:
cat /proc/config.gz | gunzip > running.config
vi running.configfor the Remoteproc drivers i have set:
#
# Remoteproc drivers
#
CONFIG_REMOTEPROC=y
CONFIG_REMOTEPROC_SRM_CORE=y
CONFIG_REMOTEPROC_SRM_DEV=y
CONFIG_STM32_RPROC=yBest regards.
2021-06-10 9:23 AM
So, as the following command
cat /proc/device-tree/mlahb/m4@10000000/m4_system_resources/statusreturn 'disabled', you certainly have somewhere in your kernel DT an overwrite of the status = "okay"; below (which is required)
&m4_rproc {
m4_system_resources {
status = "okay";
};
};Please check the order of DT includes as only last values set are taken into account.
As your are using ByteEngine SOM DT, maybe worth to talk to them.
Regards.
2021-06-13 10:38 PM
Hello PatrickF,
after we managed to enable the m4_system_resources the SPI1 clock works with PLL3_Q.
Thanks for your help.
Best regards.
2021-06-14 12:00 AM
Hi,
nice to see it was finally working.
Regards.
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.