STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

OpenSTLinux Testing

We are using OpenSTLinux as base distro for configuring and developing product on a custom STM32MP1 based embedded board. We plan to develop some testing and validation plans for the same. Just wanted to understand what sort of testing is carried out...

NPal.2 by Senior
  • 2069 Views
  • 2 replies
  • 0 kudos

Resolved! What is the correct Linux pin control configuration for ANA0 and ANA1 on TFBGA361?

I have a design based on the STM32MP157C (technically the Octavo SiP) which simulatenously uses PA0, PA1, ANA0, and ANA1. While measuring analog signals on the device, I'm noticing that the CPU is biasing the ANA0 and ANA1 signals -- based on a measu...

MWalk.3 by Associate II
  • 2801 Views
  • 3 replies
  • 1 kudos

stm32mp1 simple frame buffer

i have following yocto build configurationBuild Configuration:BB_VERSION          = "1.42.0"BUILD_SYS           = "x86_64-linux"NATIVELSBSTRING     = "universal"TARGET_SYS          = "arm-openstlinux_weston-linux-gnueabi"DISTRO              = "openst...

Ara.1 by Senior
  • 6985 Views
  • 6 replies
  • 0 kudos

What is the machine type constant to be used for booting Linux in STM32MP1 (STM32MP157F-EV1)?

Hello,   I am working on a custom Boot Loader (SSBL) for the STM32MP157F-EV1 board to replace U-Boot in the boot chain (BL33), this is a requirement for my project.   As I understand, to boot the Linux Kernel it is needed to provide 3 values through ...

AGamb.4 by Associate III
  • 1656 Views
  • 1 replies
  • 0 kudos

HAL_SPI_TransmitReceive_DMA() is not showing any data transmissiom or reception.(slave: Arduino nano as dummy sensor and stm32mp157C as master )

hello,I'm a new member here so if i am uploading this question in a wrong way please notify me.i am working at the moment with octavo board OSD32MP15x that integrates the STM32MP15x dual core Arm cortex A7 and an arm cortex m4.i am trying to run a si...

AWhic.1 by Associate
  • 996 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.