2024-10-05 6:31 PM
I did flash "stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26" image to this STM32MP135F-DK.
Boot is good, every screen like website noticed, terminal work fine.
But ssh doesn't work, attached the error message.
Then I try create new user, but change to new user, even ifconfig command doesn't work, only work for default root user.
compare with Beaglebone black, this board software is too bad.
Reagrds,
Richard Li
2024-10-06 3:54 AM
Hello Richard,
the message shown in the attached pictures is sent by the SSH server.
As far as I know it is sent if the SSH client is not known by the server.
If you confirm the question with Y the connection should be established.
Best wishes,
Edmund
2024-10-06 10:11 AM
Hi,Edmund,
Thank you!
I did try use PSFTP, it work.
There is one more issue for create user, new user no function, so I keep it open.
Best regards,
Richard
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.