2025-01-28 7:33 PM
Hi, I want to use the M4 core to handle all Audio DSP work
I can see that MXCube allows the SAI ports to be enabled on the M4 core
But it appears the I2S ports are not.
I am Missing something here
Unfortunately the Pins I need to be the PZ0-1-2-3 as PCB is done
Else If Its only possible to use the I2S from the Linux A7 then is it even possible to transfer audio data between the cores?
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.