2025-03-05 12:22 AM - last edited on 2026-01-05 1:33 AM by ELABI.1
Hello! everyone.
//-------------- Host -------------
OS: Ubuntu 22.04
Kernel: Linux leonsu-MINIPC-VC66-C2 6.8.0-52-generic
//----------- board ----------
STM32MP257F-DK
kernel: Linux stm32mp2-e3-aa-db 6.6.48
//-----------------------------------------
I followed the STM32MPU Developer Package[1] and X-LINUX-QT Expansion Package[2] to setup up the SDK and X-LINUX-QT Developer Package, respectively.
SDK Version: 6.0.0
X-LINUX-QT Developer Package Version: 2.0.1
I try to build qt example followed the section 7.1[2], I get some error message in following:
/home/leonsu/STM32MPU-Ecosystem/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/libexec/aarch64-ostl-linux/gcc/aarch64-ostl-linux/13.3.0/ld: warning: libicui18n.so.72, needed by /home/leonsu/STM32MPU-Ecosystem/Developer-Package/SDK/sysroots/cortexa35-ostl-linux/usr/lib/libQt6Core.so.6.5.3, not found (try using -rpath or -rpath-link)
/home/leonsu/STM32MPU-Ecosystem/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/libexec/aarch64-ostl-linux/gcc/aarch64-ostl-linux/13.3.0/ld: warning: libicuuc.so.72, needed by /home/leonsu/STM32MPU-Ecosystem/Developer-Package/SDK/sysroots/cortexa35-ostl-linux/usr/lib/libQt6Core.so.6.5.3, not found (try using -rpath or -rpath-link)
/home/leonsu/STM32MPU-Ecosystem/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/libexec/aarch64-ostl-linux/gcc/aarch64-ostl-linux/13.3.0/ld: /home/leonsu/STM32MPU-Ecosystem/Developer-Package/SDK/sysroots/cortexa35-ostl-linux/usr/lib/libQt6Core.so.6.5.3: undefined reference to `ucnv_getFromUCallBack_72'
........
/home/leonsu/STM32MPU-Ecosystem/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/libexec/aarch64-ostl-linux/gcc/aarch64-ostl-linux/13.3.0/ld: /home/leonsu/STM32MPU-Ecosystem/Developer-Package/SDK/sysroots/cortexa35-ostl-linux/usr/lib/libQt6Core.so.6.5.3: undefined reference to `uenum_next_72'
/home/leonsu/STM32MPU-Ecosystem/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/libexec/aarch64-ostl-linux/gcc/aarch64-ostl-linux/13.3.0/ld: /home/leonsu/STM32MPU-Ecosystem/Developer-Package/SDK/sysroots/cortexa35-ostl-linux/usr/lib/libQt6Core.so.6.5.3: undefined reference to `ucal_setMillis_72'
collect2: error: ld returned 1 exit status
gmake[2]: *** [CMakeFiles/KDABBoatDemo.dir/build.make:305: KDABBoatDemo] Error 1
gmake[1]: *** [CMakeFiles/Makefile2:88: CMakeFiles/KDABBoatDemo.dir/all] Error 2
gmake: *** [Makefile:91: all] Error 2
the version of libicu70 in SDK is libicui18n.so.74 not match to libicui18n.so.72, show in following
How do I fix the error.
Thank in advance.
reference:
1.STM32MPU Developer Package, https://wiki.st.com/stm32mpu/wiki/STM32MPU_Developer_Package
2.X-LINUX-QT Expansion Package, https://wiki.st.com/stm32mpu/wiki/X-LINUX-QT_Expansion_Package
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.