2022-04-21 12:13 AM
Hi,
I am using an official STM32MP157C-DK2 board.
I tested to build OP-TEE 3.17.0 for stm32mp1 however the boot hangs.
I am building OP-TEE OS using:
make PLATFORM=stm32mp1 \
CROSS_COMPILE_core=arm-linux-gnueabihf- \
CROSS_COMPILE_ta_arm64=arm-linux-gnueabihf- \
CFG_ARM32_core=y \
CROSS_COMPILE_ta_arm32=arm-linux-gnueabihf- \
CFG_TEE_CORE_LOG_LEVEL=2 \
CFG_TEE_CORE_DEBUG=n \
CFG_EMBED_DTB_SOURCE_FILE=stm32mp157c-dk2.dtsThe full image (st-image-core) I am using is based on meta-st-stm32mp and open-stlinux (dunfell branch)
The kernel is the one present in the meta layer: kernel (5.10.61)
I am aware that an existing version of OP-TEE is present in the build however it's from version 3.12.0.
I tried to build OP-TEE OS version 3.16.0 apart and include it in the final image and it works as expected.
I investigated and the issue comes from the linux-stm32mp kernel patches because when I built the stable kernel based on the same version 5.10.61 without patches, it works with OP-TEE 3.17.0 without issues.
My main questions are:
Thanks for your help
Solved! Go to Solution.
2022-05-10 2:22 AM
Hi @syedelec ,
This is some answer to your questions :
Main differences is that linux-stm32mp is fully integrated/tested on our STM32MP15 plaftorm and in combination with the related BSP element.
ST always recommend to use ecosystem as a whole : BSP + Kernel.
Likely some customization related to ST platform and integration strategy.
Cannot answer to this. Whatever mainline or ST version, you can find some means and tools to setup a secure platform.
But security breach or vulnerability are responsibility of product developer which integrate all pieces together.
ST will soon release ecosystem 4.0 with OPTEE 3.16 and Kernel 5.15.
Hope it help
Olivier
2022-05-10 2:22 AM
Hi @syedelec ,
This is some answer to your questions :
Main differences is that linux-stm32mp is fully integrated/tested on our STM32MP15 plaftorm and in combination with the related BSP element.
ST always recommend to use ecosystem as a whole : BSP + Kernel.
Likely some customization related to ST platform and integration strategy.
Cannot answer to this. Whatever mainline or ST version, you can find some means and tools to setup a secure platform.
But security breach or vulnerability are responsibility of product developer which integrate all pieces together.
ST will soon release ecosystem 4.0 with OPTEE 3.16 and Kernel 5.15.
Hope it help
Olivier
2022-05-10 2:30 AM
Thank you so much for your reply!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.