2021-04-27 3:36 AM
Hello everyone, i want to onfigure my stm machine on yocto using the meta-st layer:
i want to make two root partitions on the sd card (since i'm using the stm32mp157c-dk2)
the root partitions i need to integrate rauc updater in my machine.
since i installed rauc the generated st-image-weston won't boot anymore. And i think it's because of the root partitions. (rauc uses two partitions to installl an update on the first one and boot from the second one).
Please help me. Thank you
2021-05-26 12:16 AM
Hi @FHami.1
You can use the STM32CubeProgrammer to create a new partition, for example in .tsv file add " P 0x14 rootfs2 FileSystem mmc0 0xA5484400 st-image-weston-openstlinux-weston-stm32mp1.ext4.
Then you need to update in /boot/mmc0_linux/stm32mp157f-dk2_extlinux.conf the root PARTUUID with the second one.
To have the PARTUUID of the new rootfs partition you can reboot your board and enter the UBOOT during the boot process.
Use the command mmc part (STM32MP> mmc part), you will have such info display on your new partition :
8 0x006aa422 0x01dacbdc "rootfs2"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
type: linux
guid: d928d2a6-9d5e-469a-a716-8f778e35243f
The PARTUUID is the guid
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.