2024-06-25 7:41 PM
Hi
I'm using the OpenSTlinux starter package.
I want to change the SSH port communicated by dropbear from 22.
Setting a file in the device and rebooted, but it doesn't change from SSH port 22.
file: /etc/default/dropbear
DROPBEAR_PORT=10022 *line added
"DROPBEAR_EXTRA_ARGS" setting will take effect after the change.
Is it possible to change the SSH port in dropbear settings?
Best regards,
Solved! Go to Solution.
2024-07-01 6:55 AM
Hello @take_4,
To change Dropbear SSH port from 22 to 10022, you need to update the following file : /lib/systemd/system/dropbear.socket:
-ListenStream=22
+ListenStream=10022
This file is also available as a symbolic link in etc folder: /etc/systemd/system/sockets.target.wants/dropbear.socket
BR,
Christophe
2024-07-01 6:55 AM
Hello @take_4,
To change Dropbear SSH port from 22 to 10022, you need to update the following file : /lib/systemd/system/dropbear.socket:
-ListenStream=22
+ListenStream=10022
This file is also available as a symbolic link in etc folder: /etc/systemd/system/sockets.target.wants/dropbear.socket
BR,
Christophe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.