2021-04-23 2:19 AM
Hi there,
I am struggling to understand and achieve a USB gadget with Mass Storage + Serial(cdc-acm) + 1 custom interface with one bulk in and one bulk out though functionfs. Every interface works fine when runs separately. Issue starts when i try to make a composite device because of the fifo configuration.
I understand there is total of 4KB Fifo as described in reference manual and is configurable for each endpoint as needed.
I believe in my case :
MSG = I need 1 BULK IN + 1 BULK OUT
CUSTOM = I need 1 BULK IN and 1 BULK OUT
CDC ACM = needs 1 BULK IN and i BULK OUT + 1 interrupt endpoint
so my requirement is only for np-tx-fifo, is this correct?
But alwasy in composite mode it fails with :
dwc2 49000000.usb-otg: dwc2_hsotg_ep_enable: No suitable fifo found
.. <<from stm32mp151.dtsi>> – and total of entries can be 952 dwords.
g-rx-fifo-size = <128>;
g-np-tx-fifo-size = <512>;
g-tx-fifo-size = <128 128 64 64 64 64 32 32>;
Can somebody please explain how to configure it properly to achieve a composite device ?
Thanks, Rishi
2021-04-27 2:58 AM
Hi @rishi2
Do you know this page of our online documentation : https://wiki.st.com/stm32mpu/wiki/USB_overview ?
I wonder if I cannot provide hints and means to go further in investigation.
Olivier
2021-10-28 3:22 AM
Is it possible to implement 1x Rndis and 2x com ports (serial ports) with the USB Composite device gadget?
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.