STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Not able to see the SPI in /dev.

we are using stm32mp157f-ev1 and we build the weston image for this board.We want to enable the SPI-1 on this boardwe had applied the following patch to enable the SPI-1+&spi1 {  +       status = "okay";  +       pinctrl-names = "default", "sleep";  ...

HVerm.3 by Associate
  • 2850 Views
  • 2 replies
  • 0 kudos

Max clock for I2C for stm32mp157a

I have several questions first one is what is the max clock for I2C, minimum is pointed at this sheet but what is the max?Again for the same sheet for the LCD-TFT controller, I will be using 1.8V LVDS display so fclk frequency will be 45 MHz max righ...

Gencay by Associate III
  • 2056 Views
  • 1 replies
  • 0 kudos

Resolved! QSPIO NOR flash connected to STM32MP153CA bank1 does not work in U-Boot. sf probe 0 fails to initialize spi flash with error -22

I cannot get the QSPI NOR-Flash to work on my custom board using an STM32MP153CA + Adesto AT25SF128 NOR flash in U-BOOT. I'm working with 5-10-dunfell-mp1-21-11-17 files included on the 3.1.0 ecosystem.The schematic section is shown below:Is not tha...

0693W00000QMZ9BQAX.png
LCast.2 by Associate II
  • 2522 Views
  • 1 replies
  • 0 kudos

Resolved! EMMC system upgrade from SD Card

Hi,my system working fine from EMMC(written through cube programmer). I also have on my board an SD-Card slot and boot configuration pins. Is it possible to upgrade the system through SD-Card to EMMC via dd if=... from rootfs?How to prepare EMMC....r...

MWoło.2 by Senior III
  • 5827 Views
  • 6 replies
  • 0 kudos

SP_MIN for V4.0.0

I've just made the switch for V4.0.0 (A-TF 2.6, Linux 5.15 but with Barebox instead of U-Boot) using Buildroot as before.I had trouble to bring the system up because of what has been changed in regard to SCMI.The DT node's compatible name was changed...

fpoussin by Associate III
  • 2526 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.