STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PWM - output during Suspend mode

HiWe are using SEEED studio 102110318 module which uses STM32MP157CAC3 processor. We want to know if there is any way we can keep processor pin PD13 pin to low state in suspend state. We want the pin to maintain low state while in sleep mode. We have...

Srini by Associate II
  • 3164 Views
  • 4 replies
  • 0 kudos

Permanent current drain from VBAT

Hi,we are using a coin cell to supply the internal RTC of an STM32MP157 when our system is unpowered.This works as expected - as long as the external supply is off. As soon as the system is powered on, the battery is discharged with >20µA.Observing t...

jvog.sen by Associate II
  • 3370 Views
  • 4 replies
  • 0 kudos

Resolved! Boot UBIFS from dataflash (nor0)

Hi Everybody,I would like to completely boot kernel 5.10-dunfell (last year) from a 64MB dataflash (nor0). No mmc0 or nand0. Compiled the correct DTS with TF-A, U-Boot and kernel, I would like to use the following TSV for STM32CubeProgrammer:#Opt ...

ATringali by Associate II
  • 5030 Views
  • 5 replies
  • 0 kudos

Using Jtag/SWD in Linux

Custom PCB, STM32MP157C chip. Linux 5.7.10. Buildroot build. No issues - Linux boots to console prompt without trouble, no errors. I can view device registers and all memory regions using Segger Jlink via SWD in both SPL and UBoot. Once Linux starts ...

info by Associate II
  • 2942 Views
  • 1 replies
  • 0 kudos

Resolved! Command “ alsamixer�? doesn't work in SDK "en.FLASH-stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15"

root@stm32mp1:~# uname -a Linux stm32mp1 5.15.24 #1 SMP PREEMPT Wed Feb 16 11:56:41 UTC 2022 armv7l armv7l armv7l GNU/Linux root@stm32mp1:~# pacmd list-sinks-inputs No PulseAudio daemon running, or not running as session daemon. root@stm32mp1:~# alsa...

mteaching by Associate III
  • 4461 Views
  • 2 replies
  • 0 kudos

How to Start Usb2 from u-boot?

hi, i'm stuck starting usbh_hs2 from u-booti can already start usbh_hs1 at boot, in order to load kernel and fs from an usb mass storage. i wish to do the same with usb_hs2, is that possible? is one configuration from DTS or from U-boot source code? ...

MBell.5 by Associate III
  • 2599 Views
  • 3 replies
  • 1 kudos

Using HAL_RTC in TouchGFX

Hello All,forgive me if this as an obvious mistake but I'm completely new to TouchGFX. I'm using STM32 MPU, with Cube, FreeRTOS and TouchGFXI have created a page in TouchGFX using the digital clock object, I have created a TickEvent to update the clo...

DPyke.1 by Associate
  • 2045 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.