cancel
Showing results for 
Search instead for 
Did you mean: 

Permanent current drain from VBAT

jvog.sen
Associate II

Hi,

we are using a coin cell to supply the internal RTC of an STM32MP157 when our system is unpowered.

This works as expected - as long as the external supply is off. As soon as the system is powered on, the battery is discharged with >20µA.

Observing the register ADC_CCR shows that VBATEN is permanently set, connecting VBAT to the ADC input and a resistor devider (as stated in Fig. 248 in the reference manual).

[Edit: removed misleading reference to ADC driver]

In my understanding VBATEN is supposed to be set only while (and shortly before) VBAT is actually sampled. Otherwise the switch as seen in Fig. 248 does not make much sense to me.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
PatrickF
ST Employee

Hi @jvog.sen​ 

please confirm you are using ecosystem v4.x (as you refer to kernel 5.15).

Check your Device Tree wrt to https://wiki.st.com/stm32mpu/wiki/ADC_device_tree_configuration#ADC_properties

I cannot check immediately, but as far as I remember I did not notice this VBAT consumption on STM32MP157F-DK2 with latest Starter Package (which I think did not define the label = "vbat" in device tree).

As far as I know, with latest ecosystem v4.1.0, the VBATEN should be shortly enabled during ADC conversions, so there should be negligible consumption on VBAT.

Maybe you miss some patches (in uBoot and kernel).

Once clarified that you are using latest deliveries, I will double check internally with experts.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
jvog.sen
Associate II

Hi Patrick,

We are still using kernel 5.10 - sorry, that was misleading.

I will test it with kirkstone as soon as I can and report again if the error persists.

Thanks for your support!

Hello @jvog.sen​ ,

Do you still have the problem?

Best Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NEW ! Sidekick STM32 AI agent, see here

Hi @Kevin HUBER​,

we did not make the switch to kirkstone yet, so I can not tell if it solves the problem.

So for now the problem persists, but has a pretty low priority on our side.

Regards

Jan

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.