2023-11-16 3:41 AM
I'm having trouble in bringing up my custom board. I've made a custom device tree using CubeMX and adding the sections as described in "Lab-MP15_FromPartNumber_To_BasicDeviceTree_with_CubeMx". I can program fsbl-boot and fip-boot, but i'm not able to boot:
E/TC:0 tzc_it_handler:79 TZC permission failure
E/TC:0 dump_fail_filter:417 Overrun violation on filter 0
E/TC:0 dump_fail_filter:420 Permission violation on filter 0
E/TC:0 dump_fail_filter:425 Violation @0xfff09000, non-secure privileged write, AXI ID 480
Also earlier in the log:
E/TC:0 0 print_probe_list:366 |- Driver stm32mp1-cpu-opp on node cpu0-opp-table failed
I've seen earlier topics on this error (@debugging), the solution was to add a 'reserved memory' section in the u-boot device tree.
I have this in my device tree, tried both 0xce000000 and 0xde000000, but I still get the error, any ideas?
Attached is the full log and de decompiled .dtb from u-boot.
Solved! Go to Solution.
2023-11-16 7:03 AM
Fixed this by replacing the fixed-regulator (as done in the workshop) in the optee dts file with the stpmic configuration of the DK2 board. The other error was due to a wrong MPU clock frequency.
2023-11-16 7:03 AM
Fixed this by replacing the fixed-regulator (as done in the workshop) in the optee dts file with the stpmic configuration of the DK2 board. The other error was due to a wrong MPU clock frequency.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.