STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UBOOT RESET ISSUE

Hello We are working on custom board with STM32MP157AAA3 Processor.In Uboot(V2023.10) we are writing 4MB of data using mw command it works fine,but while displaying the data using md command the board resets after displaying 80KB of data.I have tried...

Resolved! Problems with DCMI DMA callback registration. Environment: MCU: STM32MP157/M4; SW: STM32Cube FW_MP1 V1.6.0; Engineering Boot Mode

Hi all!Environment: I use MX to configure the DCMI Peripheral including DMA!MX generates MX_DMA_Init() and MX_DCMI_Init()After DCMI initialization in main with the above mentioned functions I use the functions HAL_DMA_RegisterCallback(&hdma_dcmi, HAL...

MLENG.1 by Associate
  • 3006 Views
  • 3 replies
  • 1 kudos

Resolved! OP-TEE version 3.19.0-stm32mp-r1.1 - enum/integer mismatch in core/mm/core_mmu.c

Hi! I have tried to compile OP-TEE version 3.19.0-stm32mp-r1.1 for the STM32MP157F-DK2 board. With the official source on STMicroelectronics OP-TEE Github repo ,but I get the following error:$ make CROSS_COMPILE=arm-none-eabi- PLATFORM=stm32mp1-157F_...

krotti42 by Associate III
  • 3128 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.