2024-04-05 3:53 AM
Hi!
I have tried to compile OP-TEE version 3.19.0-stm32mp-r1.1 for the STM32MP157F-DK2 board. With the official source on STMicroelectronics OP-TEE Github repo ,but I get the following error:
$ make CROSS_COMPILE=arm-none-eabi- PLATFORM=stm32mp1-157F_DK2 all
GEN out/arm-plat-stm32mp1/core/include/generated/arm32_sysreg.h
[...]
CC out/arm-plat-stm32mp1/core/mm/core_mmu.o
core/mm/core_mmu.c:1514:6: error: conflicting types for 'core_mmu_get_mem_by_type' due to enum/integer mismatch; have 'void(unsigned int, vaddr_t *, vaddr_t *)' {aka 'void(unsigned int, long unsigned int *, long unsigned int *)'} [-Werror=enum-int-mismatch]
1514 | void core_mmu_get_mem_by_type(unsigned int type, vaddr_t *s, vaddr_t *e)
| ^~~~~~~~~~~~~~~~~~~~~~~~
In file included from core/include/mm/tee_pager.h:13,
from core/include/mm/fobj.h:11,
from core/include/mm/sp_mem.h:10,
from core/arch/arm/include/kernel/secure_partition.h:14,
from core/include/kernel/user_mode_ctx.h:11,
from core/mm/core_mmu.c:19:
core/include/mm/core_mmu.h:535:6: note: previous declaration of 'core_mmu_get_mem_by_type' with type 'void(enum teecore_memtypes, vaddr_t *, vaddr_t *)' {aka 'void(enum teecore_memtypes, long unsigned int *, long unsigned int *)'}
535 | void core_mmu_get_mem_by_type(enum teecore_memtypes type, vaddr_t *s,
| ^~~~~~~~~~~~~~~~~~~~~~~~
cc1: note: unrecognized command-line option '-Wno-c2x-extensions' may have been intended to silence earlier diagnostics
cc1: all warnings being treated as errors
make: *** [mk/compile.mk:163: out/arm-plat-stm32mp1/core/mm/core_mmu.o] Error 1
$ I have modified core/mm/core_mmu.c successfully, but currently not tested on the real board.
Patch:
diff -ruN STMicroelectronics_3.19.0-stm32mp-r1.1/core/mm/core_mmu.c STMicroelectronics_3.19.0-stm32mp-r1.1_fixed/core/mm/core_mmu.c
--- STMicroelectronics_3.19.0-stm32mp-r1.1/core/mm/core_mmu.c 2024-04-05 12:18:40.298370873 +0200
+++ STMicroelectronics_3.19.0-stm32mp-r1.1_fixed/core/mm/core_mmu.c 2024-04-05 12:20:44.152661288 +0200
@@ -1511,7 +1511,7 @@
/*
* teecore gets some memory area definitions
*/
-void core_mmu_get_mem_by_type(unsigned int type, vaddr_t *s, vaddr_t *e)
+void core_mmu_get_mem_by_type(enum teecore_memtypes type, vaddr_t *s, vaddr_t *e)
{
struct tee_mmap_region *map = find_map_by_type(type);
Kind regards
Solved! Go to Solution.
2024-05-24 5:57 AM
Hi @PatrickF
This error is when building the OP-TEE with GCC version >=13. For building I used this description mentioned in the ST Wiki.
Here you can find the corresponding commit in the official (vanilla) OP-TEE repo which fix this issue:
$ git-log core/mm/core_mmu.c
[...]
commit 359c54b79de65acb91a50acd20d28a166c448510
Author: Jose Quaresma <jose.quaresma@foundries.io>
Date: Mon Jun 12 18:32:24 2023 +0100
core: mm: Fix conflicting types due to enum/integer mismatch
This is an error with gcc13 [-Werror=enum-int-mismatch]
Reviewed-by: Jens Wiklander <jens.wiklander@linaro.org>
Signed-off-by: Jose Quaresma <jose.quaresma@foundries.io>
[...]
$
2024-05-24 5:19 AM
Hi @krotti42
did you look at https://wiki.st.com/stm32mpu/wiki/How_to_configure_OP-TEE
Regards.
2024-05-24 5:57 AM
Hi @PatrickF
This error is when building the OP-TEE with GCC version >=13. For building I used this description mentioned in the ST Wiki.
Here you can find the corresponding commit in the official (vanilla) OP-TEE repo which fix this issue:
$ git-log core/mm/core_mmu.c
[...]
commit 359c54b79de65acb91a50acd20d28a166c448510
Author: Jose Quaresma <jose.quaresma@foundries.io>
Date: Mon Jun 12 18:32:24 2023 +0100
core: mm: Fix conflicting types due to enum/integer mismatch
This is an error with gcc13 [-Werror=enum-int-mismatch]
Reviewed-by: Jens Wiklander <jens.wiklander@linaro.org>
Signed-off-by: Jose Quaresma <jose.quaresma@foundries.io>
[...]
$
2024-05-27 9:11 AM
Hi,
OpTee patch will be present in upcoming OpenSTLinux Ecosystem Rev.5.1
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.