STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! No STM32 device in DFU mode connected

Hi all, I'm trying to customize the device tree of the stm board, but I'm stuck early on. I'm trying to follow stm32mp157c-dk2 tutorial to flash Starter Package (https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Package), however, ...

Jaglaz by Associate II
  • 7386 Views
  • 7 replies
  • 0 kudos

Resolved! EV1 & MB1379 Performance

Hello ST Teams!I'd like to know if someone have ever tried to get 1920*1080*30fps with the configuration above (STM32MP157C-EV1 and MB1379 board). We'd like to achieve this performance, OV5640 datasheet camera says "ok for me"v4l2 listing capabiliti...

Eldam by Senior
  • 3316 Views
  • 2 replies
  • 0 kudos

Increased boot time when using FIP

Hello,   We are upgrading from BSP 2.1.0 to 3.0.0. With BSP 2.1.0 we had implemented a Secure Boot mechanism as described here, i.e. both TF-A and u-boot were signed with the STM32 Signing Tool and had a stm32 header added.   Now with BSP 3.0.0 we se...

Hi, I have built the OpenSTLinux distribution according to your wiki guide (https://wiki.st.com/stm32mpu/index.php/STM32MP1_Distribution_Package#Building_the_OpenSTLinux_distribution).

I want to populate the distribution to an SD-card and mount it in STM32MP157A-DK1 according to this link: https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer#How_to_populate_a_microSD_card_inserted_in_a_Linux_host_PCMy host PC is a virtual machine ...

JMour.1 by Associate II
  • 5719 Views
  • 6 replies
  • 0 kudos

Resolved! OpenAMP_FreeRTOS example vs Cube Project - Why is the Cube project putting the init for IPCC and OpenAMP is the else section of the Is_Engineering_Boot_Mode() if statement?

I created a project using CUBEIDE for STM32MP157C-DK2 and set all peripherals to initialize. I enabled FreeRTOS and then started porting over the example code in in the Projects folder for the OpenAMP_FreeRTOS_echo application. It is all compiling ...

Resolved! "ums 0 mmc 0" doesn't work

Hello,I can't use the "ums" command via terminalprog (minicom)Message is always"STM32MP> ums 0 mmc 0UMS: LUN 0, dev 0, hwpart 0, sector 0x0, count 0x1dacc00Please connect USB cable. "After 60 seconds: "USB cable not detected. Command exit."Communicat...

MEige by Associate II
  • 2490 Views
  • 2 replies
  • 0 kudos

Mounting userfs on /home?

HiIn my project the root filesystem is read-only, so I need to have a writeable partition mounted on /home. I first tried doing this in my machine conf (conf/machine/stm32mp1-raichu.conf) with the following lines:ST_VENDORFS = "0" ST_USERFS = "1" S...

Resolved! STM32MP157CA SPI1 Clock does not work

We use the STM32MP157CA and the STM32CubeIDE and let the code generator generate a confiuration with the required modules. In our case the SPI1 on the pins (PZ0,PZ1,PZ2). The generated functions provide the initializations for the SPI1. Unfortunately...

DBaes.1 by Associate III
  • 11392 Views
  • 18 replies
  • 0 kudos

STM32MP157 hangs at INFO: SP_MIN: Preparing exit to normal world while exiting standby mdoe

When exiting out of standby mode through RTC,Wakeup pins or PON Key in all the cases System stops at : INFO:  SP_MIN: Preparing exit to normal world.Here is the complete log :[  32.488278] usb33: supplied by vdd_usb#echo mem > /sys/power/state [  37...

rishi2 by Associate III
  • 3023 Views
  • 4 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.