2021-06-15 11:45 AM
Hello,
I can't use the "ums" command via terminalprog (minicom)
Message is always
"STM32MP> ums 0 mmc 0
UMS: LUN 0, dev 0, hwpart 0, sector 0x0, count 0x1dacc00
Please connect USB cable. "
After 60 seconds: "USB cable not detected. Command exit."
Communication via minicom/ST-Link and ETH works.
STM32MP> usb start
starting USB...
USB0: USB EHCI 1.00
scanning bus 0 for devices... 2 USB Device(s) found
scanning usb for storage devices... 0 Storage Device(s) found
System is buildroot, an older one and a version with kernel 5.8. No difference.
I can't find the mistake.
Marc
Solved! Go to Solution.
2021-06-16 8:16 AM
Hello Olivier,
the missing and a wrong USB cable was the problem. One of the USB cables is for charging/power supply only. And that cable was connected to the OTG.
The datalines of such cables are not connected inside. This type of cable is cheaper to manufacture. It's a commone trap (Many Type B cables suffer from this problem also). The problem is solved.
Thank you for your help.
Marc
2021-06-16 1:34 AM
Hello MEige (Community Member)
Do you use a custom board or an ST board? If you use an STM32MP157C-DK2 board, after "STM32MP> ums 0 mmc 0" just plug an USB OTG type C cable as mentioned to open an USB mass storage device in U-boot. What happens when you do so?
Regards,
Olivier
2021-06-16 8:16 AM
Hello Olivier,
the missing and a wrong USB cable was the problem. One of the USB cables is for charging/power supply only. And that cable was connected to the OTG.
The datalines of such cables are not connected inside. This type of cable is cheaper to manufacture. It's a commone trap (Many Type B cables suffer from this problem also). The problem is solved.
Thank you for your help.
Marc
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.