2022-10-25 9:43 AM
I am using the stm32wb55 as a Central.
When pairing to my server, I encounter long pairing times.
About 80 seconds from the moment I send the passkey to the time I get paired complete event.
.
(I have no errors in the pairing complete event)
I did not have this issue with my previous device. Pairing has always been done quickly.
Please tell me if I might be doing something wrong. What might be prolonging the process?
2022-10-28 10:41 AM
Hello,
Is this delay increasing depending on the number of connections in your setup? Which connection interval are you using?
Best Regards
2022-10-30 5:35 AM
Thanks. I checked and the connection interval was way too long, after changing it all works fine.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.