2025-05-05 4:53 AM - edited 2026-05-11 7:55 AM
Hi
I was here with a timer question not long ago, and everything seemed solved. https://community.st.com/t5/stm32-mcus-wireless/timer-tim2-does-not-work-when-ble-is-initialized-in-stm32wb55/m-p/794896#M24405
I am working on a custom device, but I made a demo version for the nucleo board to share the project.
Respected @FilipKremen helped me then. Also, when regenerating the project with entering standby mode, everything crashed, and for many days, I couldn't find what the problem was because most of the files seemed to be identical. And now I added the functionality with the standby mode to the project with the timer example, and I was able to trace the problem.
If I activate #define CFG_LPM_SUPPORTED 1, entering standby mode on a long press of button 1 works, but the timer doesn't start at the initialization.
At the same time, if CFG_LPM_SUPPORTED is 0, the timer works fine, but entering standby mode does not work.
Is this a bug, or am I missing something? Please help me
I am attaching a project for the Nucleo board
Solved! Go to Solution.
2025-05-12 5:07 AM
Hello,
this is probably because the tasks for entering standby mode are registered in APP_BLE_Init() and this function is called during BLE initialization, so the tasks aren't registered in the sequencer yet.
Best regards,
ST support
2025-05-12 5:20 AM
Yes, that's right, I forgot about that. Thank you very much!!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.