2025-05-24 8:20 PM
Hello,
I'm trying to flash the example program in B-WL5M-SUBG1 connectivity expansion board, and below issue.
Tried with different EVK boards but still the persists.
I got a popup for updating firmware of STLINK-V3MINIE debugger, so I upgraded the firmware from V3J8M3 to version V3J16M7 before flashing the hardware.
Above is the screenshot taken after the firmware upgrade.
Regards,
Prakash N
2025-06-27 8:28 AM
Hello @PrakashN
Could you please try using the STM32CubeProg V2.19.0 or the STM32CubeIDE V1.18.1. If you still have issue, please describe the connection and the HW setup of both ST-LINK and B-WL5M-SUBG1.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.