2025-06-10 7:33 AM - edited 2025-06-17 12:28 AM
Hello,
We made a custom pcb with STM32WLE5CC MCU, and with the IPD BALFHB-WL-05D3. You'll find in attachement the schematic.
We use the STM32CubeWL software. We tries the same version on the nucleo and everityhing was going well, we could join with the nucleo (Nucleo WL55JC2)
We would like some support to find out why we could not join the network, and why there is CRC error.
Our Gateway is a Multitech MTCDT-H5-210L Firmware 5.3.8s-s1
Thank you for your help
Anthony
EDIT : The problem came from the 32 MHz quartz, which had a slightly low frequency. We solved the problem with the internal capacity of the microcontroller
Solved! Go to Solution.
2025-06-12 3:35 AM - edited 2025-07-03 4:22 AM
Hello @Anthony Plantin
The NUCLEO-WL55JC2 is designed to work on low band frequencies. But for the BALFHB-WL-05D3, it is a IPD used for High band STM32WL designs. So, this may be way the same SW is refusing to connect. Could you please check this.
PS: The problem came from the 32 MHz quartz, which had a slightly low frequency. You can solve the problem with the internal capacity of the microcontroller
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-06-12 3:35 AM - edited 2025-07-03 4:22 AM
Hello @Anthony Plantin
The NUCLEO-WL55JC2 is designed to work on low band frequencies. But for the BALFHB-WL-05D3, it is a IPD used for High band STM32WL designs. So, this may be way the same SW is refusing to connect. Could you please check this.
PS: The problem came from the 32 MHz quartz, which had a slightly low frequency. You can solve the problem with the internal capacity of the microcontroller
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-06-12 3:40 AM
@Anthony Plantin wrote:why there is CRC error.
What CRC error?
@Anthony Plantin wrote:Our Gateway is a Multitech MTCDT-H5-210L Firmware 5.3.8s-s1
Does it give you any diagnostics indicating what's failed, and why?
2025-10-07 1:10 AM
Hello there,
The problem came from the load capacitors of the lse quartz. The timing was wrong, and caused a join fail. We managed to solve the problme with the internal trimming capacitor.
Thank you for your help
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.