2025-10-07 1:25 AM
Hello everyone,
I am trying to communicate via LoRaWAN on the live object network of the French operator Orange. I'm using the nucleo STM32WL55 for the end device.
Here are the version of the application on the end device side :
APPLICATION_VERSION: V1.3.1
MW_LORAWAN_VERSION: V2.6.1
MW_RADIO_VERSION: V1.3.1
L2_SPEC_VERSION: V1.0.3
RP_SPEC_VERSION: V1-1.0.3
I tried with these two lora mac version :
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.