2021-03-16 1:13 AM
Hi all.
I found out there are specific DEBUG_SUBGHZSPI_* alternate functions (DS13105 STM32WLE5xx)
.
But there is not much information about these functions.
Can these AF be used to 'mirror' SUBGHZSPI pins for debugging / captures ?
Thanks
Olivier
2021-04-20 7:30 AM
Hi,
in Core/Src/sys_debug.c, these pins can be activated with by setting the DEBUGGER_ON to 1
Please, see the code below:
/*Radio Spi Dbg on PA4/5/6/7*/
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Pin = (GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_7);
GPIO_InitStruct.Alternate = GPIO_AF13_DEBUG_SUBGHZSPI;
__HAL_RCC_GPIOA_CLK_ENABLE();
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* Busy on PA12*/
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Pin = (GPIO_PIN_12);
GPIO_InitStruct.Alternate = GPIO_AF6_RF_BUSY;
__HAL_RCC_GPIOA_CLK_ENABLE() ;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.