2023-11-30 1:57 AM
STM32WL lorawan middleware use a RTC subsecond underflow interrupt update tick instead systick,but the subsecond underflow interrupt never entered.It seems interrupt not enabled, so I manually enable RTC subsecond underflow interrupt but the handler still never accessed.
/* RTC init function */
void MX_RTC_Init(void)
{
/* USER CODE BEGIN RTC_Init 0 */
/* USER CODE END RTC_Init 0 */
RTC_TimeTypeDef sTime = {0};
RTC_DateTypeDef sDate = {0};
RTC_AlarmTypeDef sAlarm = {0};
/* USER CODE BEGIN RTC_Init 1 */
/* USER CODE END RTC_Init 1 */
/** Initialize RTC Only
*/
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = RTC_PREDIV_A;
hrtc.Init.SynchPrediv = RTC_PREDIV_S;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
hrtc.Init.OutPutPullUp = RTC_OUTPUT_PULLUP_NONE;
hrtc.Init.BinMode = RTC_BINARY_NONE;
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN Check_RTC_BKUP */
/* USER CODE END Check_RTC_BKUP */
/** Initialize RTC and set the Time and Date
*/
sTime.Hours = 0x0;
sTime.Minutes = 0x0;
sTime.Seconds = 0x0;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_RESET;
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
{
Error_Handler();
}
sDate.WeekDay = RTC_WEEKDAY_MONDAY;
sDate.Month = RTC_MONTH_JANUARY;
sDate.Date = 0x1;
sDate.Year = 0x0;
if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
{
Error_Handler();
}
/** Enable the Alarm A
*/
sAlarm.AlarmTime.Hours = 0x0;
sAlarm.AlarmTime.Minutes = 0x0;
sAlarm.AlarmTime.Seconds = 0x0;
sAlarm.AlarmTime.SubSeconds = 0x0;
sAlarm.AlarmTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sAlarm.AlarmTime.StoreOperation = RTC_STOREOPERATION_RESET;
sAlarm.AlarmMask = RTC_ALARMMASK_NONE;
sAlarm.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_ALL;
sAlarm.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_DATE;
sAlarm.AlarmDateWeekDay = 0x1;
sAlarm.Alarm = RTC_ALARM_A;
if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BCD) != HAL_OK)
{
Error_Handler();
}
/** Enable the WakeUp
*/
if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0, RTC_WAKEUPCLOCK_RTCCLK_DIV16, 0) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN RTC_Init 2 */
/* USER CODE END RTC_Init 2 */
}
void HAL_RTC_MspInit(RTC_HandleTypeDef* rtcHandle)
{
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
if(rtcHandle->Instance==RTC)
{
/* USER CODE BEGIN RTC_MspInit 0 */
/* USER CODE END RTC_MspInit 0 */
/** Initializes the peripherals clocks
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_RTC;
PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
/* RTC clock enable */
__HAL_RCC_RTC_ENABLE();
__HAL_RCC_RTCAPB_CLK_ENABLE();
/* RTC interrupt Init */
HAL_NVIC_SetPriority(RTC_WKUP_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(RTC_WKUP_IRQn);
HAL_NVIC_SetPriority(RTC_Alarm_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(RTC_Alarm_IRQn);
/* USER CODE BEGIN RTC_MspInit 1 */
/* USER CODE END RTC_MspInit 1 */
}
}
PS: As far, I can’t find any configuration about subsecond underflow interrupt in CubeMX and any code snippet in offical example project.
2023-12-05 3:00 AM
Hello Simon,
Some points that are not included in the code you provided :
Additionally, by default, Cube MX sets the wake-up counter to 0. You should modify it to a value such as 0x0800, which will give you an interrupt every second with the wake-up clock selected with RTC/16.
Best Regards,
Victor
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.