2025-09-27 7:08 PM
Hello,
I'm chasing a problem where my project is having its configuration of SMPS mode switch back to LDO, and I was realizing that the settings are reset when USB is enabled. Digging into this, I came across this:
/* Enable VDDUSB */
if(__HAL_RCC_PWR_IS_CLK_ENABLED())
{
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWREx_EnableVddUSB();
HAL_PWREx_EnableUSBPWR();
__HAL_RCC_PWR_CLK_DISABLE();
}
else
{
HAL_PWREx_EnableVddUSB();
}At a glance, the logic appears incorrect -- why would you enable PWR_CLK when you just checked and it was already enabled? I looked through the v1.7.0 SDK example projects, and saw that most other projects, the line is `if (__HAL_RCC_PWR_IS_CLK_ENABLED() != 1U)`. This only appears here:
./Projects/NUCLEO-WBA65RI/Applications/USBX/Ux_Device_CDC_ACM/Core/Src/stm32wbaxx_hal_msp.c: if(__HAL_RCC_PWR_IS_CLK_ENABLED())
./Projects/NUCLEO-WBA65RI/Applications/USBX/Ux_Device_CDC_ACM/Core/Src/stm32wbaxx_hal_msp.c: if(__HAL_RCC_PWR_IS_CLK_ENABLED())
./Projects/NUCLEO-WBA65RI/Applications/USBX/Ux_Host_HID/Core/Src/stm32wbaxx_hal_msp.c: if(__HAL_RCC_PWR_IS_CLK_ENABLED())
./Projects/NUCLEO-WBA65RI/Applications/USBX/Ux_Host_HID/Core/Src/stm32wbaxx_hal_msp.c: if(__HAL_RCC_PWR_IS_CLK_ENABLED())
./Projects/NUCLEO-WBA65RI/Applications/USBX/Ux_Device_HID_Standalone/Core/Src/stm32wbaxx_hal_msp.c: if(__HAL_RCC_PWR_IS_CLK_ENABLED())
./Projects/NUCLEO-WBA65RI/Applications/USBX/Ux_Device_HID_Standalone/Core/Src/stm32wbaxx_hal_msp.c: if(__HAL_RCC_PWR_IS_CLK_ENABLED())
./Projects/NUCLEO-WBA65RI/Applications/USBX/Ux_Host_HID_Standalone/Core/Src/stm32wbaxx_hal_msp.c: if(__HAL_RCC_PWR_IS_CLK_ENABLED())
./Projects/NUCLEO-WBA65RI/Applications/USBX/Ux_Host_HID_Standalone/Core/Src/stm32wbaxx_hal_msp.c: if(__HAL_RCC_PWR_IS_CLK_ENABLED())Is this indeed a bug?
Thank you,
Jonathan
Solved! Go to Solution.
2025-09-29 8:10 AM
Hello @JFisher-Legato
After checking internally, I think the following changes should be made both in HAL_PCD_MspInit and HAL_PCD_MspDeinit:
This should be solved on the same internal ticket i've already created.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-28 6:02 AM - edited 2025-09-29 3:15 AM
Hello @JFisher-Legato
I think this is a typo. It must be:
(__HAL_RCC_PWR_IS_CLK_ENABLED() != 1U)
And not:
__HAL_RCC_PWR_IS_CLK_ENABLED()
I've escalated this internally to be updated on the future (under internal ticket number 218518).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-28 7:45 AM
Thank you - that does appear to help a bit. Then the next question I have is why there seems to be a missing call to
HAL_PWREx_EnableUSBPWR();I have enabled this and things seem to be better.
Additionally, the logic is also backwards in the HAL_PCD_DeInit() call.
2025-09-29 8:10 AM
Hello @JFisher-Legato
After checking internally, I think the following changes should be made both in HAL_PCD_MspInit and HAL_PCD_MspDeinit:
This should be solved on the same internal ticket i've already created.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.