2025-07-25 5:36 AM
Hi,
I'm working on a project using the STM32WB5MMG, which supports up to 4 simultaneous BLE connections.
When a central device enables or disables notifications, my firmware receives the corresponding events (NOTIFY_ENABLED_EVT / NOTIFY_DISABLED_EVT) inside the Custom_STM_App_Notification() function. However, I'm unsure whether the ConnectionHandle parameter in this context reliably identifies which central device triggered the change.
Additionally, when the firmware updates a characteristic's value using Custom_STM_App_Update_Char(), we know we must wait for the CUSTOM_STM_NOTIFICATION_COMPLETE_EVT (handled in custom_app.c) before sending the next notification.
Now that we're dealing with multiple central devices, here's my main concern:
Does CUSTOM_STM_NOTIFICATION_COMPLETE_EVT include the specific ConnectionHandle of the device that received the last notification?
If not, how can we safely coordinate and track per-connection notification completion to avoid sending notifications out of order?
I'd appreciate guidance on whether the SDK handles this internally per connection or if I need to implement a custom per-connection queue or state tracker.
Thanks!
2025-09-01 5:27 AM
Hello @netanelu
According to the BLE spec, the only way to notify a specific central device is to disable the notification for all other central devices.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.