2024-12-08 7:59 AM
Hello,
I face same issue.
same as
https://community.st.com/t5/stm32-mcus-wireless/stm32wb-cpu1-stuck-waiting-cpu2-at-init/td-p/80505
I am use the BLE_Ota on STM32WB5MM-DK,
set CFG_LED_SUPPORTED = 0, CFG_BUTTON_SUPPORTED = 0
I tried to Commenting these lines as last post same.
and it's not working.
I still stuck waiting for SHCI_C2_BLE_Init() to finish after APP send Reboot.
On P-NUCLEO-WB55 is working well.
On STM32WB5MM-DK is stuck. (but erase user application from 0x8007000, only BLE_Ota can do FUOTA by APP without Reboot)
Any help from anyone would be greatly appreciated.
Thanks,
Leimen
Debug log as follow:
----------------------------------------
Wireless Firmware version 1.13.2
Wireless Firmware build 2
FUS version 1.2.0
>>== SHCI_SUB_EVT_CODE_READY
>>== WIRELESS_FW_RUNNING
>>== DBGMCU_GetRevisionID= 2003
>>== DBGMCU_GetDeviceID= 495
Success: SHCI_C2_BLE_Init command
==>> Start Ble_Hci_Gap_Gatt_Init function
Success: hci_reset command
Success: aci_hal_write_config_data command - CONFIG_DATA_PUBADDR_OFFSET
Public Bluetooth
Address: xx:xx:xx:xx:xx:xx
Success: aci_hal_write_config_data command - CONFIG_DATA_IR_OFFSET
Success: aci_hal_write_config_data command - CONFIG_DATA_ER_OFFSET
Success: aci_hal_set_tx_power_level command
Success: aci_gatt_init command
Success: aci_gap_init command
Success: hci_le_set_default_phy command
Success: aci_gap_set_io_capability command
Success: aci_gap_set_authentication_requirement command
Success: aci_gap_configure_whitelist command
==>> End Ble_Hci_Gap_Gatt_Init function
Success: aci_hal_set_radio_activity_mask command
==>> aci_gap_set_discoverable - Success
==>> Success
Start Fast Advertising
>>== HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE - Connection handle: 0x801
- Connection established with Central: @:xx:xx:xx:xx:xx:xx
- Connection Interval: 30.00 ms
- Connection latency: 0
- Supervision Timeout: 5000 ms
>>== HCI_LE_CONNECTION_UPDATE_COMPLETE_SUBEVT_CODE
- Connection Interval: 7.50 ms
- Connection latency: 0
- Supervision Timeout: 5000 ms
>>== HCI_LE_CONNECTION_UPDATE_COMPLETE_SUBEVT_CODE
- Connection Interval: 30.00 ms
- Connection latency: 0
- Supervision Timeout: 5000 ms
-- P2P APPLICATION SERVER : NOTIFICATION ENABLED
-- GATT : REBO?
Wireless Firmware version 1.13.2
Wireless Firmware build 2
FUS version 1.2.0
>>== SHCI_SUB_EVT_CODE_READY
>>== WIRELESS_FW_RUNNING
>>== DBGMCU_GetRevisionID= 2003
>>== DBGMCU_GetDeviceID= 495
Success: SHCI_C2_BLE_Init command
==>> Start Ble_Hci_Gap_Gatt_Init function
Success: hci_re
set command
Success: aci_hal_write_config_data command - CONFIG_DATA_PUBADDR_OFFSET
Public Bluetooth Address: xx:xx:xx:xx:xx:xx
Success: aci_hal_write_config_data command - CONFIG_DATA_IR_OFFSET
Success: aci_hal_write_config_data command - CONFIG_DATA_ER_OFFSET
Success: aci_hal_set_tx_power_level command
Success: aci_gatt_init command
Success: aci_
gap_init command
Success: hci_le_set_default_phy command
Success: aci_gap_set_io_capability command
Success: aci_gap_set_authentication_requirement command
Success: aci_gap_configure_whitelist command
==>> End Ble_Hci_Gap_Gatt_Init function
Success: aci_hal_set_radio_activity_mask command
==>> aci_gap_set_discoverable - Success
==>> Success: Start Fast Advertising
2024-12-08 8:09 AM
append
2024-12-08 8:15 AM
P-NUCLEO-WB55
STM32WB5MM-DK
2025-01-15 6:50 AM - edited 2025-02-21 8:47 AM
Hello @Leimen1007
Could you please try to update the Stack using the .bin files available on the last version of the STM32CubeWB V1.21.0.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.