2023-04-18 5:07 AM
Hi to all.
I have a problem whit USB dongle STM32WB55.
With BLE stack and all BLE examples from STM32Cube_FW_WB_V1.16.0 Virtual USB port is working just fine.
But when I change to stm32wb5x_Zigbee_FFD_fw and use P-NUCLEO-WB55.USBDongle\Applications\Zigbee\Zigbee_OnOff_Server_Coord Virtual USB port is not working (error code 10). I can turn on and off LED form coordinator (dongle) to router (Nucleo board), and virtual port on Nucleo is working just fine. But virtual port on dongle is not working (erorr code 10).
My OS is Win10, I updated Virtual serial port drivers, I changed CDC_DATA_HS_MAX_PACKET_SIZE to 64U but again I have the same problem.
Can you please help me.
Thanks.
Solved! Go to Solution.
2023-04-20 11:17 AM
WOW thank you Remy !!!!!
It is alive :beaming_face_with_smiling_eyes:
Besides adding second parameter I add
static uint8_t VcpRxBuffer[MAX_DBG_TRACE_MSG_SIZE];
And it is working!
Thanks again.
2023-04-19 10:02 AM
Hello,
When you call VCP_Init function, a null pointer is give as second parameter, instead this null pointer, give a rx buffer in parameter like this:
VCP_Init( &VcpTxBuffer[0], &VcpRxBuffer[0] );
Best Regards
2023-04-20 11:17 AM
WOW thank you Remy !!!!!
It is alive :beaming_face_with_smiling_eyes:
Besides adding second parameter I add
static uint8_t VcpRxBuffer[MAX_DBG_TRACE_MSG_SIZE];
And it is working!
Thanks again.
2023-06-27 9:31 AM
Hi, I don't know if this problem is related.
I'm developing a work at Board Nucleo-WB55RG. I already get the Zigbee communication and USB communication working well on the board, but when I merge them in the same project, I have some problems.
My PC identify the USB connection, but in the same project, when I put available the Zigbee on middleware STM32WPAN on the IOC file, I lost this USB connection. So, my PC doesn't identify any more the USB connection after that. Does someone know if there is some conflict between the USB communication and Zigbee on Nucleo-Wb55RG? Or can I solve my problem?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.