STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WL workshop material generates errors with CubeMX

Hello, I'm practicing the "Point to Point Phy layer application lab" in the "MOOC STM32WL workshop" series.After downloading the material and opening the project with CubeIDE and building the project, everything is fine. however, when I try to add a ...

0693W00000bhVMrQAM.png 0693W00000bhVPaQAM.png
AElgh by Associate III
  • 3809 Views
  • 7 replies
  • 0 kudos

STM32WB55 not able to commission/pair with Matter.

I have flash Matter code from [ stm32-hotspot/stm32wb-matter-device-over-thread ] into STM32WB55 board.I have Matter Hub Device with OTBR, Command Line Chip-Tool and Android Mobile Chip-Tool Application is ready and functioning with other Matter End ...

VMODI.1 by Associate II
  • 3156 Views
  • 4 replies
  • 0 kudos

Resolved! Bugs in the stm32wlxx_hal_rtc.c file.

In my opinion there are two bugs HAL_RTC_SetTime(..) (p. 776) and HAL_RTC_GetTime(..) (p. 881)./* Check Binary mode ((32-bit free-running counter) */if (READ_BIT(RTC->ICSR, RTC_ICSR_BIN) != RTC_BINARY_ONLY)should be RTC_BINARY_ONLY instead of RTC_BIN...

ANalb.1 by Associate
  • 2236 Views
  • 3 replies
  • 0 kudos

On STM32WB55CG, after sending "RX_start 1" to coprocessor CM4 threads starts to respond significantly slower. Can this issue be caused by stm32wb5x_Phy_802_15_4_fw.bin itself?

We have human interface board based on STM32WB55CG with planned possibility to communicated with other nodes via ZigBee. Now we have to pass the RF certification for which specific driver communicating with coprocessor was implemented. Most of comman...

Resolved! BLE and USB-CDC with FreeRTOS

I have a project which has the requirement of BLE and USB in CDC mode. The implementation is done with the FreeRTOS. BLE and USB are working independently, but when I integrate both of them in a single project then there are some issues which are bei...

ABN by Associate III
  • 3542 Views
  • 5 replies
  • 1 kudos

About STM32WL55

HiI am testing SUBGHZ with STM32WL55I activated IPCC of System Core and SUBGHZ of Connectivity.and then I enabled SUBGHZ_PHY of Middleware and Software Packs​I generated code and compiled.When I run the program, it halted. ​It enter the Error_Handler...

wake up CPU1 from CPU2

Hi,in my application on STM32WL55, when the CPU1 (CM4) is on STANDBY mode, and the CPU2 (CM0PLUS) is in Run mode,how can i ask the CPU2 to wakeup the CPU1 ?Thank you.

malarab by Senior II
  • 920 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.