2023-01-26 9:32 AM
Hi,
I try to start a a continuous waveform (CW) from the STM32WB radio using theaci_hal_tone_start command from the DTM suite. I execute the following commands:
hci_reset( );
HAL_Delay( 10 );
aci_hal_set_tx_power_level( 1, tx_pow );
aci_hal_tone_start( RF_Channel, offset);
which all return success.
At that point the ble advertisements stop so it is doing something, but I do not seem to be getting the CW.
Am I missing some call to eg 'activate; DTM ?
Or something else I might be doing wrong ?
(I looked at the PER testbench code, but did not see anything special in the start_TX function of that codebase, there the same steps are done except of course the different last call to start transmitting packets)
Thanks
Bram
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.