2023-01-25 3:21 PM
* JLink Info: Device "STM32WB55VG" selected.
JLink info:
------------
DLL: V7.66d, compiled Jun 21 2022 17:00:22
Firmware: J-Link Ultra V4 compiled Sep 24 2021 16:41:09
Hardware: V4.00
Feature(s) : RDI, FlashBP, FlashDL, JFlash, GDB
* JLink Info: Found SW-DP with ID 0x6BA02477
* JLink Info: Failed to power up DAP
* JLink Info: Found SW-DP with ID 0x6BA02477
* JLink Info: DPIDR: 0x6BA02477
* JLink Info: CoreSight SoC-400 or earlier
* JLink Info: Scanning AP map to find all available APs
* JLink Info: AP[0]: Stopped AP scan as end of AP map seems to be reached
* JLink Info: Iterating through AP map to find AHB-AP to use
***JLink Error: Could not find core in Coresight setup
Error: Flash Download failed - Target DLL has been cancelled
How can I fix it?
2023-01-26 1:16 AM
Hello @Community member ,
Try to boot from system memory.
If you use the STM32CubeIDE, please refer to UM2609 and precisely Debug using SEGGER J-Link Section and check the debug configuration.
I hope this help you!!
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.