2021-07-08 6:52 AM
Hello!
I'm using stm32wb nucleo board as a central device to connect multiple peripherals. An input data stream from one device is about 40 kb/s, there can be up to three devices. After successful connection the client board starts to get notifications. But at some point the central device stops processing events - such as ACI_GATT_NOTIFICATION_VSEVT_CODE, HCI_DISCONNECTION_COMPLETE_EVT_CODE etc (it could be 10 minutes, half hour or several hours). I know for sure that peripherals continue to transmit data. After this I can't disconnect peripherals, start discover or other ble actions. But as I can see in debugger peripheral stay connected. I have not found a reason why this happens and solution for this problem.
Maybe someone had the same issue?
Best regards,
Den
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.