2025-06-10 11:15 AM - last edited on 2025-06-11 2:29 AM by STTwo-32
Hello,
I am using p-nucleo-wb55. I have a code with an RTC alarm interrupt triggered every 5 seconds. In the ISR, I set a sequencer task that sends a message via BLE. I have enabled the LPM as I want the MCU to enter sleep mode while it isn't working and only wakeup with the RTC alarm. I realized that the MCU doesn't stay in the sleep mode and when I debug, I realized that it wakes up so fast as the IPCC RX Interrupt is triggered continuously with high frequency.
How can I control this, knowing that I don't need the MCU to do any task through those 5 seconds, I just want it to sleep and wakeup only after 5 seconds.
Thanks in advance
Solved! Go to Solution.
2025-08-05 7:28 AM - edited 2025-08-05 9:55 AM
Hello @FilipKremen
Yes, I have checked and I can't find a solution to my problem.
Why shouldn't I add code in the main? I just put it in to make it easier to detect whether the MCU enters sleep mode or keeps blinking.
2025-08-06 12:35 AM
Hello,
the LED keeps blinking because BLE advertising is running and it wakes up the MCU. If you comment this line Adv_Request(APP_BLE_FAST_ADV); in app_ble.c file, it stops blinking.
I recommend reading low power section in STM32WB55 datasheet. (3.7.5)
Best regards,
Filip Kremen
2025-08-07 1:40 AM
Hello @MahmoudAhmed11
I have a configuration similar to yours in which I only need to transmit the data contained in the advertisement.
I'll try to explain to you what I did, I hope you understand.
In the Adv_Cancel function, I added:
/* USER CODE BEGIN Adv_Cancel_2 */
activeFlag = false;
LL_C2_PWR_SetPowerMode(LL_PWR_MODE_SHUTDOWN);
/* USER CODE END Adv_Cancel_2 */activeFlag is a boolean global variable (initialized to false)
Then I have the function:
static void Adv_Cancel_Req(void) {
/* USER CODE BEGIN Adv_Cancel_Req_1 */
/* USER CODE END Adv_Cancel_Req_1 */
UTIL_SEQ_SetTask(1 << CFG_TASK_ADV_CANCEL_ID, CFG_SCH_PRIO_0);
/* USER CODE BEGIN Adv_Cancel_Req_2 */
/* USER CODE END Adv_Cancel_Req_2 */
return;
}
And the function:
void Adv_Start(void) {
// ... manufacturer specific data update (into advertising array)
/**
* Start to Advertise to be connected by a Client
*/
Adv_Request(APP_BLE_FAST_ADV);
HW_TS_Start(myTimerFlag, (ADVERTISING_TIMEOUT_MS * 1000 / CFG_TS_TICK_VAL));
return;
}
In the APP_BLE_Init() function, I added:
/* USER CODE BEGIN APP_BLE_Init_2 */
HW_TS_Create(CFG_TIM_STOP_ADV, &(myTimerFlag), hw_ts_SingleShot, Adv_Cancel_Req);
/* USER CODE END APP_BLE_Init_2 */
In the while(1) loop, I don't directly call the MX_APPE_Process() function, but I call a state machine whose main states are:
This ensures that the device functions correctly. Each time I invoke the transmission procedure, packets are sent for a time equal to ADVERTISING_TIMEOUT_MS (I set it to 1000, or 1 second).
I hope the explanation is clear and that it can be of help to you.
What I haven't been able to achieve, however, is achieve similar behavior when enabling the Eddystone TML Beacon protocol (in STM32CubeMX: BT SIG Beacon = EDDYSTONE_TLM_BEACON).
I hope someone can help me.
2025-09-05 8:06 AM
Thanks @FilipKremen @STTwo-32 @mgatti
The problem has been solved by cancelling the advertisement before entering the sleep mode and starting it again after waking up.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.