2025-07-31 3:58 AM
Good day
I am trying to run the Lorawan FUOTA demo on my nucleo-wl55jc1 and havinf trouble.
Once i build files in the recommended order and they build successfully, i am getting this issue:
struggling to find out what i need to change in order for it to work. I am using cubeIDE version 1.19.0.
Please assist as we plan into going into production very soon on our own PCB board.
Solved! Go to Solution.
2025-08-29 3:21 AM
Hello @HKhan.4;
To solve the build issue with STM32CubeIDE 1.19.0 version, I recommend you to add this instruction under 1_Image_KMS_Blob/Application/User/kms_blob_example_keys.c file:
__attribute__((weak)) void _close(void){}
__attribute__((weak)) void _lseek(void){}
__attribute__((weak)) void _read(void){}
__attribute__((weak)) void _write(void){}
or you can copy syscalls.c and sysmem.c files from \STM32Cube_FW_WL_V1.3.1\Projects\NUCLEO-WL55JC\Applications\LoRaWAN_FUOTA\1_Image_SECoreBin\STM32CubeIDE\Application\User and paste under STM32Cube_FW_WL_V1.3.1\Projects\NUCLEO-WL55JC\Applications\LoRaWAN_FUOTA\1_Image_KMS_Blob\STM32CubeIDE\Application\User
I hope this help you to solve the build issue.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-31 4:02 AM
when I use the script, i get this issue:
###########################################
# 0- Set all global variables
###########################################
###########################################
# 1- Compile all BFU projects
###########################################
Create.
Opening '1_Image_KMS_Blob'.
Building All Projects...
13:00:52 **** Clean-only build of configuration Debug for project 1_Image_KMS_Blob ****
make -j20 clean
rm -rf ./Application/User/kms_blob_example_keys.cyclo ./Application/User/kms_blob_example_keys.d ./Application/User/kms_blob_example_keys.o ./Application/User/kms_blob_example_keys.su
rm -rf KMS_Blob.bin KMS_Blob.elf KMS_Blob.list KMS_Blob.map default.size.stdout
13:00:52 Build Finished. 0 errors, 0 warnings. (took 445ms)
13:00:52 **** Build of configuration Debug for project 1_Image_KMS_Blob ****
make -j20 all
arm-none-eabi-gcc "C:/Users/42410/STM32Cube/Repository/STM32Cube_FW_WL_V1.3.1/Projects/NUCLEO-WL55JC/Applications/LoRaWAN_FUOTA/1_Image_KMS_Blob/Src/kms_blob_example_keys.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32WL55xx -DCORE_CM4 -DDEBUG -c -I../../../../../../../Drivers/STM32WLxx_HAL_Driver/Inc -I../../../../../../../Drivers/STM32WLxx_HAL_Driver/Inc/Legacy -I../../../../../../../Drivers/CMSIS/Device/ST/STM32WLxx/Include -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/BSP/STM32WLxx_Nucleo -I../../../../../../../Middlewares/ST/STM32_Key_Management_Services/Core -I../../../1_Image_SECoreBin/Inc -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/kms_blob_example_keys.d" -MT"Application/User/kms_blob_example_keys.o" --specs=nano.specs -mfloat-abi=soft -mthumb -o "Application/User/kms_blob_example_keys.o"
arm-none-eabi-gcc -o "KMS_Blob.elf" @"objects.list" -mcpu=cortex-m4 -T"C:\Users\42410\STM32Cube\Repository\STM32Cube_FW_WL_V1.3.1\Projects\NUCLEO-WL55JC\Applications\LoRaWAN_FUOTA\1_Image_KMS_Blob\STM32CubeIDE\KMS_Blob.ld" --specs=nosys.specs -Wl,-Map="KMS_Blob.map" -Wl,--gc-sections -static --specs=nano.specs -mfloat-abi=soft -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m/nofp\libc_nano.a(libc_a-closer.o): in function `_close_r':
(.text._close_r+0xc): warning: _close is not implemented and will always fail
C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m/nofp\libc_nano.a(libc_a-closer.o): note: the message above does not take linker garbage collection into account
C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m/nofp\libc_nano.a(libc_a-lseekr.o): in function `_lseek_r':
C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m/nofp\libc_nano.a(libc_a-lseekr.o): note: the message above does not take linker garbage collection into account
(.text._lseek_r+0x10): warning: _lseek is not implemented and will always fail
C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m/nofp\libc_nano.a(libc_a-readr.o): in function `_read_r':
(.text._read_r+0x10): warning: _read is not implemented and will always fail
C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m/nofp\libc_nano.a(libc_a-readr.o): note: the message above does not take linker garbage collection into account
C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m/nofp\libc_nano.a(libc_a-writer.o): in function `_write_r':
(.text._write_r+0x10): warning: _write is not implemented and will always fail
C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m/nofp\libc_nano.a(libc_a-writer.o): note: the message above does not take linker garbage collection into account
Finished building target: KMS_Blob.elf
arm-none-eabi-size KMS_Blob.elf
arm-none-eabi-objdump -h -S KMS_Blob.elf > "KMS_Blob.list"
arm-none-eabi-objcopy -O binary KMS_Blob.elf "KMS_Blob.bin"
text data bss dec hex filename
1200 0 0 1200 4b0 KMS_Blob.elf
Finished building: default.size.stdout
Finished building: KMS_Blob.list
Finished building: KMS_Blob.bin
"../postbuild.sh" ".." "KMS_Blob" "1"
Windows_NT
prepareimage with windows executable
C:/Users/42410/STM32Cube/Repository/STM32Cube_FW_WL_V1.3.1/Middlewares/ST/STM32_Secure_Engine/Utilities/KeysAndImages/win/prepareimage/prepareimage.exe enc -k ../../Binary/OEM_KEY_COMPANY1_key_AES_CBC.bin -i ../../Binary/iv.bin KMS_Blob.bin ../../Binary/KMS_Blob.kmsu
C:/Users/42410/STM32Cube/Repository/STM32Cube_FW_WL_V1.3.1/Middlewares/ST/STM32_Secure_Engine/Utilities/KeysAndImages/win/prepareimage/prepareimage.exe sha256 KMS_Blob.bin ../../Binary/KMS_Blob.sign -p 16
C:/Users/42410/STM32Cube/Repository/STM32Cube_FW_WL_V1.3.1/Middlewares/ST/STM32_Secure_Engine/Utilities/KeysAndImages/win/prepareimage/prepareimage.exe pack -k ../../Binary/ECCKEY.txt -m KMSB -r 28 -v 1 -i ../../Binary/iv.bin -f ../../Binary/KMS_Blob.kmsu -t ../../Binary/KMS_Blob.sign -o 320 ../../Binary/KMS_Blob.kmsb
13:00:57 Build Failed. 4 errors, 4 warnings. (took 4s.840ms)
2025-08-29 3:21 AM
Hello @HKhan.4;
To solve the build issue with STM32CubeIDE 1.19.0 version, I recommend you to add this instruction under 1_Image_KMS_Blob/Application/User/kms_blob_example_keys.c file:
__attribute__((weak)) void _close(void){}
__attribute__((weak)) void _lseek(void){}
__attribute__((weak)) void _read(void){}
__attribute__((weak)) void _write(void){}
or you can copy syscalls.c and sysmem.c files from \STM32Cube_FW_WL_V1.3.1\Projects\NUCLEO-WL55JC\Applications\LoRaWAN_FUOTA\1_Image_SECoreBin\STM32CubeIDE\Application\User and paste under STM32Cube_FW_WL_V1.3.1\Projects\NUCLEO-WL55JC\Applications\LoRaWAN_FUOTA\1_Image_KMS_Blob\STM32CubeIDE\Application\User
I hope this help you to solve the build issue.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-04 5:18 AM
Hi
Thank you for this. I was able to complete the build but i am still running into issues. Please refer to the ticket below:
https://community.st.com/t5/stm32-mcus-wireless/lorawan-fuota/td-p/832920
Please let me know when I can possibly have feedback.
2025-09-05 7:36 AM
Hello @HKhan.4,
Thank you for updating post.
Glad to know that the initial issue is solved and you are able to build the project without issue.
For that, please click on Accept as Solution on the reply which solved your issue.
For the second issue, I will share the second post with wireless team expert.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.