2021-08-28 1:29 PM
From the STM32CubeWB firmware package, there is a Thread_RCP project. However, there doesn't seem to be any documentation for it (it is not even mentioned in AN5289). The only hint is the readme.txt file which says:
"This application is used to demonstrate the OpenThread Border router feature using an STM32WB device.
To play with the demo, you need a Raspberry Pi 3B (RPi) to perform the link with Wi-Fi/Ethernet networks
The full setup and the associated documentations can be requested to ST on demand".
Where can I find the full setup and associated documentation?
Thank you,
2022-11-19 10:29 PM
@Remi QUINTIN
Appreciated if you can advise on this?
2022-11-20 7:53 AM
the document has 13 pages; just download it . :)
2022-11-20 4:01 PM
The documentation says this, so I'm asking.
A full configured RPi image is provided by ST.
Please get the OTBR_CLI_RPi_1.0.img.
Regards
2022-11-20 4:02 PM
2024-02-07 12:33 PM
I'm also looking for the OTBR_CLI_RPi_1.0.img downloading sources for my students (educational HE project).
Is there any info I'm missing? All documentation links stating "get ... file" are inactive.
Best regards,
Piotr
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.